We have a simple button in a library, which has 4 pads, but only 2 pins in
schematic. Always, 2 and 2 pads are connected internally inside the button
part. Let's say pads 12 are connected togeher and 34 as well. I would like
to be able to connect either to pin 1 or pin 2 in board layout, so I could
use the internal 1-2 connection as a jumper or bridger or how you call it.
It seems that I always have an air connection between the pins 1 and 2.
Is there any cure to this?
Thank you,
Petr