EAGLE User Support (English) importing sch and board into project
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
  • Replies 4 replies
  • Subscribers 178 subscribers
  • Views 384 views
  • Users 0 members are here
Related

importing sch and board into project

autodeskguest
autodeskguest over 17 years ago

Hi,

 

Is it possible to import a schematic and board layout from one eagle cad

project into another?  I have a circuit and placed layout that I would

like to maintain the layout of and paste into another schematic/board.

 

cheers,

Jamie

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    Jamie Morken schrieb:

     

    Is it possible to import a schematic and board layout from one eagle cad

    project into another?  I have a circuit and placed layout that I would

    like to maintain the layout of and paste into another schematic/board.

     

    The easiest way is to start the new design from a copy of the old one.

     

    If that is not possible, you must GROUP/CUT/PASTE the schematic and

    board parts separately, and for this temporarily close the other editor

    window to turn annotation off. After having copied both parts, open the

    second editor again and run ERC. Be prepared to fix some (eventually

    many) inconsistencies.

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    Hi,

     

    the help file list the following for the PASTE command:

     

    wrote in message

    news:g139gc$nbv$1@cheetah.cadsoft.de...

    Jamie Morken schrieb:

     

    Is it possible to import a schematic and board layout from one eagle cad

    project into another?  I have a circuit and placed layout that I would

    like to maintain the layout of and paste into another schematic/board.

     

    The easiest way is to start the new design from a copy of the old one.

     

    If that is not possible, you must GROUP/CUT/PASTE the schematic and

    board parts separately, and for this temporarily close the other editor

    window to turn annotation off. After having copied both parts, open the

    second editor again and run ERC. Be prepared to fix some (eventually

    many) inconsistencies.

     

    Tilmann

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    Hello Tilmann Reh !:

    Is it possible to import a schematic and board layout from one eagle cad

    project into another?  I have a circuit and placed layout that I would

    like to maintain the layout of and paste into another schematic/board.

     

    The easiest way is to start the new design from a copy of the old one.

     

    Be careful. If the source design was made by an illegal Eagle copy you

    have to expect some serious troubles in the future.

     

    I am not sure but maybe CadSoft willchange this philosophy. At the

    moment it is better to be extremely careful.....

     

    regards

    --

    Grzegorz Zalot

     

    complex ltd.

    office tel/fax : +48 32 2505840

    mobil : +48 501 301515

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    Carsten Wille wrote:

    Hi,

     

    the help file list the following for the PASTE command:

     

    <quote>

    Function

    Copies the contents of the paste buffer to a drawing.

     

    Syntax

     

    PASTE .

     

    Mouse keys

     

    Center mirrors the contents of the paste buffer.

    Right rotates the contents of the paste buffer.

     

    See also CUT, GROUP

     

    Using the commands GROUP, CUT, and PASTE, parts of a drawing/library can be

    copied to the same or different drawings/libraries. When using the PASTE

    command, the following points should be observed:

     

      a.. CUT/PASTE cannot be used in device editing mode.

      b.. Elements and signals on a board can only be copied to a board.

      c.. Elements, buses and nets on a schematic can only be copied to a

    schematic.

      d.. Pads and smds can only be copied from package to package.

      e.. Pins can only be copied from symbol to symbol.

      f.. When copying elements, signals, pads, smds and pins, a new name is

    allocated if the previous name is already used in the new drawing.

      g.. Buses retain the same names.

      h.. Nets retain the same name as long as one of the net segments has a

    label. If no label is present, a new name is generated if the previous name

    is already in use.

    If there are modified versions of devices or packages in the paste buffer,

    an automatic library update will be started to replace the objects in the

    schematic or board with the ones from the paste buffer. Note: You should

    always run a Design Rule Check (DRC) and an Electrical Rule Check (ERC)

    after a library update has been performed!

     

    </quote>

     

     

     

    As Tilmann wrote, you have to cut and paste separately schematic and board.

    But the clue is the last item in the bullet list: Eagle's behavoir of

    renaming nets.

     

    My way of doubling parts of board and schematic is:

     

    step0: Make a backup just in case.

     

    step1: Have both, sch and brd open. Use the schematic to edit.

     

    step2: Name all signals (and I mean really all) with a net name that ends on

    a letter. E.g. N$17 -> N$17A. All copied net name will change from N$17A to

    N$17A1 etc.

     

    step3: Attach label to all signals you do not want to change in the copy.

    (Esp. VCC and GND)

     

    step4: Save

     

    I've only really found the  net re-naming to be necessary when I took a

    design , deleted a lot of it, to give the section I wanted to copy, and then

    went to do the copy /paste routine. As the net names  were not continuous

    this threw up a few problems and a lot of inconsitencies crept in...

     

    In most cases with a reasonabley fresh design this stage is not required.

     

    However if you do want to re-name all your nets then have a look at the

    ULP's in merge_brd.zip.

     

    One renames all nets by adding a suffix automatically.

     

    The other is a re-name ULP for components that also allows for an offset in

    the number to be added. IN many situations renaming the components is

    important to ensure you have a clean sequence with no holes in it, which can

    throw up some problems occasionally.

     

     

    I didn't write either of these ULPs- just modified them to meet my own

    requirements at the time.

     

    there are a couple of other ulps that look interesting but I've not used them

     

    cheers

     

    David