Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) symbol with multiple package variations
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 177 subscribers
  • Views 556 views
  • Users 0 members are here
Related

symbol with multiple package variations

autodeskguest
autodeskguest over 17 years ago

Is there a way to allow, for instance any logic device that uses a DIL14

package to be able to use a variation on that package that has been created

without having to go through the entire logic family individually with the

variation device table linking the symbol with the package? For instance,

with Protel one can double click the symbol in a schematic and specify the

package that is used.

Thanks in anticipation of a reply.

Don

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    "Gary Gofstein" <ggofstein@lbl_nospam.gov> schrieb im Newsbeitrag

    news:g2msm2$ftf$1@cheetah.cadsoft.de...

    I still do not understand your problem, if I have an opamp that has thru

     

    I see you respond to Don Owen, but allow me to jump in again....

     

    hole and SMD package variations, and I want to change the package but

    maintain the same part, that is easily changeable by the method I

    described: on your layout, use the change command, select package, click

    your part and you will be given a choice of which package to use.

     

    Of course this only works if the package has already been tied to that

    particular part in the library.

     

    Exactly, and this is the point.

     

    It is not true ( in general) that the pins for the different packages will

    always correspond, so pin 2 on the DIL package may not be connected to

    the same node as pin 2 on the SOIC package.

     

    This clearly is within the designer's responsibility. I do not want to be

    forced into useless library work just because there is a slight chance that

    the pin numbering scheme does not correspond in some cases. Simply because

    the risk is not the least bit lower if you do it all through the libraries.

    This is a waste of time. Did you ever work with Eagle V3.5? I am still

    working with it today for most of the time, although I have all licenses up

    to V5, and this is one of the reasons.

     

    Although, if you mostly use logic, you may never have come across this.

    This is the reason why you may have to use the "connect" dialog in the

    library to link a particular part to a new package. In general, there is

    no one to one correspondence. If you doubt this I can send you some

    examples!

     

    I know, and I tell you this added "connect" complexity through the use of

    the library editor is worth absolutely nothing. I already had these

    discussions. My answer in the past was that you can do exactly the same

    mistake within the library editor: In V3.5 you could replace a package with

    another. Trouble arose if the pin numbering was different. Today you have to

    define and "connect" a new package in the library editor. Just as easily you

    can take over the (wrong) pin assignment from another package. The only

    difference here is the increased effort. Again, this is a time waster. It is

    even more likely that you are so busy with the definition of the new

    packages in the library editor that you miss the actual problem with the non

    matching numbering. With the "REPLACE" I start to think about this at

    exactly the right time, and I am not distressed by this package definition

    nonsense inside the lib editor.

     

     

    I am very confused by your posting. It seems that you are saying you wish

    there was another layer of package specification so that all 14DIL

    packages could be substituted for one another. So you could have a 14DIL

    with big and with small holes, or 8SOIC with two pad variations, one for

    wave and one for hand soldering? Then they would always correspond, so

    there would be no need to specify where the signals come out on each

    package pin? Is this what you're saying?

     

    Basically, I can't tell if your just overlooking the admittedly obtuse way

    (that most things are in EAGLE) of changing packages simply and easily.

    Or, if you really have a problem that EAGLE's package substitution won't

    solve and also don't appreciate that there is no way to generally

    substitute one package for another. Or, perhaps I have no clue as to what

    you're talking about and your problem would instantly make sense to me

    once I understood what, exactly, you are trying to do.

     

    As I pointed out elsewhere: if we both were to update the same board by

    replacing a number of components (say, from SO footprint to TSSOP), and you

    do it with V5 or V4, while I do it with V3.5, I can promise you that you are

    still busy defining the first two packages, when I already finished my job,

    closed my office and made myself a nice tea.

     

    T.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago in reply to autodeskguest

    So you weren't really looking for "support" so much as you are asking

    for a new feature, or more accurately the removal of a "misfeature".

     

    Well, I never used v3 of EAGLE, so I guess I don't know how much more

    easily it handles this problem for you.

     

    In my case, the packages rarely have any significant correspondence, so

    I am quite happy with the connect dialog. It takes me only a few seconds

    to connect up those 8 op amp pins while I glance at the data sheet. My

    bottleneck is remembering how to copy other packages into the library if

    they are not already present.

     

    Maybe the new pins in the connect dialog should default to the pads that

    are already defined for the part. Then you'd only have to click OK if

    they match up. That would save you 2 mouse clicks per pad. I could see

    that if you have a package with dozens or hundreds of pins that match

    up, it would make real sense.

     

    Again, I'll stress, my situation is the exact opposite of yours, the

    packages do not correspond, so I love the connection dialog. But I

    generally support your view, the software doesn't need to babysit or

    think for  the user. Maybe I'll download 3.5 and try it! Go have a nice tea!

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago in reply to autodeskguest

    So you weren't really looking for "support" so much as you are asking

    for a new feature, or more accurately the removal of a "misfeature".

     

    Well, I never used v3 of EAGLE, so I guess I don't know how much more

    easily it handles this problem for you.

     

    In my case, the packages rarely have any significant correspondence, so

    I am quite happy with the connect dialog. It takes me only a few seconds

    to connect up those 8 op amp pins while I glance at the data sheet. My

    bottleneck is remembering how to copy other packages into the library if

    they are not already present.

     

    Maybe the new pins in the connect dialog should default to the pads that

    are already defined for the part. Then you'd only have to click OK if

    they match up. That would save you 2 mouse clicks per pad. I could see

    that if you have a package with dozens or hundreds of pins that match

    up, it would make real sense.

     

    Again, I'll stress, my situation is the exact opposite of yours, the

    packages do not correspond, so I love the connection dialog. But I

    generally support your view, the software doesn't need to babysit or

    think for  the user. Maybe I'll download 3.5 and try it! Go have a nice tea!