Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) symbol with multiple package variations
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 177 subscribers
  • Views 556 views
  • Users 0 members are here
Related

symbol with multiple package variations

autodeskguest
autodeskguest over 17 years ago

Is there a way to allow, for instance any logic device that uses a DIL14

package to be able to use a variation on that package that has been created

without having to go through the entire logic family individually with the

variation device table linking the symbol with the package? For instance,

with Protel one can double click the symbol in a schematic and specify the

package that is used.

Thanks in anticipation of a reply.

Don

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

     

    "Gary Gofstein" <ggofstein@lbl_nospam.gov> schrieb im Newsbeitrag

    news:g2s6c4$93l$1@cheetah.cadsoft.de...

    So you weren't really looking for "support" so much as you are asking for

    a new feature, or more accurately the removal of a "misfeature".

     

    Well, I never used v3 of EAGLE, so I guess I don't know how much more

    easily it handles this problem for you.

     

    All these little additional steps add up to a significant amount of

    superfluous work, which is why I still work with V3.5 wherever possible. And

    I am not too happy about it.

     

    In my case, the packages rarely have any significant correspondence, so I

    am quite happy with the connect dialog.

     

    You may be surprised - but I agree!

     

    It takes me only a few seconds to connect up those 8 op amp pins while I

    glance at the data sheet.

     

    Be honest: at this time you already fired up the LIB editor, entered a

    device, added another package, opened up the connect dialog... and you still

    did nothing on the board itself!

     

    My bottleneck is remembering how to copy other packages

    into the library if they are not already present.

     

    David was already so kind to point this out for you, it's pretty simple. But

    to make this clear: of course the connect dialog is an important part of the

    component management, and I am not trying to get rid of it. Point is, I do

    not like to be forced into this sort of work for the straightforward

    replacements, in many cases the pin numbering is perfectly identical. In

    other cases you need minor individual modifications to packages, all leading

    to additional package variants in V4/V5. In V3.5 you had one library for

    these individual things, without the need to link those to your devices.

    Picking up on David's mentioned comment with the "copy" feature in the

    connect dialog (which is useful, no doubt): in most situations where one

    copies the connection it would have been way easier to REPLACE the package

    directly. The way it is today may appear convenient to you, but you would be

    surprised how much simpler this was in the old V3.5 days!!

     

    Maybe the new pins in the connect dialog should default to the pads that

    are already defined for the part. Then you'd only have to click OK if they

    match up. That would save you 2 mouse clicks per pad. I could see that if

    you have a package with dozens or hundreds of pins that match up, it would

    make real sense.

     

    Again: in those cases I do not want to mess with devices and its packages, I

    do not want to see a connect dialog, I do not even want to enter the library

    editor. In V3.5 you picked a TSSOP14 from somewhere, clicked on your

    existing SO14, and you were done. The process couldn't be any simpler or

    faster, don't you think?

     

    Again, I'll stress, my situation is the exact opposite of yours, the

    packages do not correspond, so I love the connection dialog. But I

     

    Nay, I confess it is not... In the course of this discussion only pronounced

    the frequent situation where such 1:1 replacements are possible. There's no

    less opportunities where you really had to add packages with different pin

    assignments which definitely require one's attention through the use of the

    library editor, but I think we do not need to mention this here. In these

    cases the tools for this work do serve the purpose, and quite efficiently.

     

    generally support your view, the software doesn't need to babysit or think

    for  the user. Maybe I'll download 3.5 and try it! Go have a nice tea!

     

    Do it - it's really worth experiencing it. Enjoy the weekend - with or

    without tea,

     

    T.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

     

    "Gary Gofstein" <ggofstein@lbl_nospam.gov> schrieb im Newsbeitrag

    news:g2s6c4$93l$1@cheetah.cadsoft.de...

    So you weren't really looking for "support" so much as you are asking for

    a new feature, or more accurately the removal of a "misfeature".

     

    Well, I never used v3 of EAGLE, so I guess I don't know how much more

    easily it handles this problem for you.

     

    All these little additional steps add up to a significant amount of

    superfluous work, which is why I still work with V3.5 wherever possible. And

    I am not too happy about it.

     

    In my case, the packages rarely have any significant correspondence, so I

    am quite happy with the connect dialog.

     

    You may be surprised - but I agree!

     

    It takes me only a few seconds to connect up those 8 op amp pins while I

    glance at the data sheet.

     

    Be honest: at this time you already fired up the LIB editor, entered a

    device, added another package, opened up the connect dialog... and you still

    did nothing on the board itself!

     

    My bottleneck is remembering how to copy other packages

    into the library if they are not already present.

     

    David was already so kind to point this out for you, it's pretty simple. But

    to make this clear: of course the connect dialog is an important part of the

    component management, and I am not trying to get rid of it. Point is, I do

    not like to be forced into this sort of work for the straightforward

    replacements, in many cases the pin numbering is perfectly identical. In

    other cases you need minor individual modifications to packages, all leading

    to additional package variants in V4/V5. In V3.5 you had one library for

    these individual things, without the need to link those to your devices.

    Picking up on David's mentioned comment with the "copy" feature in the

    connect dialog (which is useful, no doubt): in most situations where one

    copies the connection it would have been way easier to REPLACE the package

    directly. The way it is today may appear convenient to you, but you would be

    surprised how much simpler this was in the old V3.5 days!!

     

    Maybe the new pins in the connect dialog should default to the pads that

    are already defined for the part. Then you'd only have to click OK if they

    match up. That would save you 2 mouse clicks per pad. I could see that if

    you have a package with dozens or hundreds of pins that match up, it would

    make real sense.

     

    Again: in those cases I do not want to mess with devices and its packages, I

    do not want to see a connect dialog, I do not even want to enter the library

    editor. In V3.5 you picked a TSSOP14 from somewhere, clicked on your

    existing SO14, and you were done. The process couldn't be any simpler or

    faster, don't you think?

     

    Again, I'll stress, my situation is the exact opposite of yours, the

    packages do not correspond, so I love the connection dialog. But I

     

    Nay, I confess it is not... In the course of this discussion only pronounced

    the frequent situation where such 1:1 replacements are possible. There's no

    less opportunities where you really had to add packages with different pin

    assignments which definitely require one's attention through the use of the

    library editor, but I think we do not need to mention this here. In these

    cases the tools for this work do serve the purpose, and quite efficiently.

     

    generally support your view, the software doesn't need to babysit or think

    for  the user. Maybe I'll download 3.5 and try it! Go have a nice tea!

     

    Do it - it's really worth experiencing it. Enjoy the weekend - with or

    without tea,

     

    T.