EAGLE User Support (English) How to print a board complete with polygon fill?
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
  • Replies 3 replies
  • Subscribers 177 subscribers
  • Views 289 views
  • Users 0 members are here
Related

How to print a board complete with polygon fill?

autodeskguest
autodeskguest over 17 years ago

I want to produce board layout artwork on my printer that has a polygon

fill. Whenever I reload the board, the fill disappears and I have to

regenerate the fill on screen. I believe that the Gerber output will

regenerate the fill but I simply want to generate artwork on my line printer

complete with fill. Have I missed the relevant section in the manual that

explains all this? Do I have to produce the Gerber outputs to achieve this

or is there a quick and easy method using just the print from the control

panel menu?

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    Thanks Tilmann,

    I have already done this, but I guess the hidden agenda of my question was

    whether the artwork produced using this is the same as that produced from

    going through the Gerber production procedure. Maybe I'm just being lazy

    trying to get some quick tips and so my next task is to produce Gerber files

    and find out for myself. I've got to say that its a pity that Eagle can't

    preserve the fill without having to click the rats nest but its not a big

    deal.

    Don

     

     

    "Tilmann Reh" wrote in message news:...

    Don Owen schrieb:

     

    I want to produce board layout artwork on my printer that has a polygon

    fill. Whenever I reload the board, the fill disappears and I have to

    regenerate the fill on screen. I believe that the Gerber output will

    regenerate the fill but I simply want to generate artwork on my line

    printer

    complete with fill. Have I missed the relevant section in the manual

    that

    explains all this? Do I have to produce the Gerber outputs to achieve

    this

    or is there a quick and easy method using just the print from the

    control

    panel menu?

     

    Polygons are stored as outlines in the design files and calculated by

    RATSNEST (see help and manual).

     

    Simply run RATSNEST once after loading your files, /then/ PRINT.

     

    (The CAMP will automatically calculate polygons when producing gerber

    output. PRINT just prints the files as they appear on the screen.)

     

    Tilmann

     

    "Tilmann Reh" <tilmannreh@despammed.com> wrote in message

    news:g2j9vb$f1s$1@cheetah.cadsoft.de...

    Don Owen schrieb:

     

    I want to produce board layout artwork on my printer that has a polygon

    fill. Whenever I reload the board, the fill disappears and I have to

    regenerate the fill on screen. I believe that the Gerber output will

    regenerate the fill but I simply want to generate artwork on my line

    printer

    complete with fill. Have I missed the relevant section in the manual that

    explains all this? Do I have to produce the Gerber outputs to achieve

    this

    or is there a quick and easy method using just the print from the control

    panel menu?

     

    Polygons are stored as outlines in the design files and calculated by

    RATSNEST (see help and manual).

     

    Simply run RATSNEST once after loading your files, /then/ PRINT.

     

    (The CAMP will automatically calculate polygons when producing gerber

    output. PRINT just prints the files as they appear on the screen.)

     

    Tilmann

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    Thanks Tilmann,

    I have already done this, but I guess the hidden agenda of my question was

    whether the artwork produced using this is the same as that produced from

    going through the Gerber production procedure. Maybe I'm just being lazy

    trying to get some quick tips and so my next task is to produce Gerber files

    and find out for myself. I've got to say that its a pity that Eagle can't

    preserve the fill without having to click the rats nest but its not a big

    deal.

    Don

     

     

    "Tilmann Reh" wrote in message news:...

    Don Owen schrieb:

     

    I want to produce board layout artwork on my printer that has a polygon

    fill. Whenever I reload the board, the fill disappears and I have to

    regenerate the fill on screen. I believe that the Gerber output will

    regenerate the fill but I simply want to generate artwork on my line

    printer

    complete with fill. Have I missed the relevant section in the manual

    that

    explains all this? Do I have to produce the Gerber outputs to achieve

    this

    or is there a quick and easy method using just the print from the

    control

    panel menu?

     

    Polygons are stored as outlines in the design files and calculated by

    RATSNEST (see help and manual).

     

    Simply run RATSNEST once after loading your files, /then/ PRINT.

     

    (The CAMP will automatically calculate polygons when producing gerber

    output. PRINT just prints the files as they appear on the screen.)

     

    Tilmann

     

    "Tilmann Reh" <tilmannreh@despammed.com> wrote in message

    news:g2j9vb$f1s$1@cheetah.cadsoft.de...

    Don Owen schrieb:

     

    I want to produce board layout artwork on my printer that has a polygon

    fill. Whenever I reload the board, the fill disappears and I have to

    regenerate the fill on screen. I believe that the Gerber output will

    regenerate the fill but I simply want to generate artwork on my line

    printer

    complete with fill. Have I missed the relevant section in the manual that

    explains all this? Do I have to produce the Gerber outputs to achieve

    this

    or is there a quick and easy method using just the print from the control

    panel menu?

     

    Polygons are stored as outlines in the design files and calculated by

    RATSNEST (see help and manual).

     

    Simply run RATSNEST once after loading your files, /then/ PRINT.

     

    (The CAMP will automatically calculate polygons when producing gerber

    output. PRINT just prints the files as they appear on the screen.)

     

    Tilmann