EAGLE User Support (English) Best technique for star grounds, Kelvin connections, etc?
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
  • Replies 2 replies
  • Subscribers 178 subscribers
  • Views 783 views
  • Users 0 members are here
Related

Best technique for star grounds, Kelvin connections, etc?

autodeskguest
autodeskguest over 17 years ago

Hello fellow Eagle users,

 

   I am working on some projects that require multiple logically

distinct netlists that actually connect on the board.  The

simple, typical situation is "digital ground" and "analog ground",

which are to be connected at a single point to avoid ground

loops.  This is often called a "star ground".  There are more

general situations, where various subsections of the board

(one per ADC, for example) need separate ground polygons which are

connected to each other with a controlled layout on the board.

 

   The issue is not limited to grounding.  Kelvin circuits,

separated force/sense lines, and a variety of other real-life

circuitry call for logically distinct netlists that connect at

controlled points on the board.

 

   At the moment, I am using Bert Menkveld's recent suggestion

of a library symbol with two pins and a device with two

superimposed pads.  This works, with several drawbacks in the

board view.  First, when preparing the board files for the

fabricator, the unwanted pads and drills have to be removed.

Second, there are lots of DRC complaints and one must be careful

not to ignore a real design rule violation in the noise of

"expected" complaints.  Third, a device mandates a through-hole

or SMD pad, even when you only want to use an inner layer.  This

places some modest restrictions on component layout.

 

   So, I am looking for recommendations on the best techniques

in Eagle for handling "star grounds", Kelvin connections, and

so on.  Currently using Eagle 4.16r2, and expect to upgrade

when our budget allows it.

 

Stu Friedberg

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    On Wed, 18 Jun 2008 20:19:08 -0700, I wrote:

    a device with two superimposed pads.

     

    A package, obviously.  Just to forestall unnecessary replies.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago

    On Wed, 18 Jun 2008 20:19:08 -0700, I wrote:

    a device with two superimposed pads.

     

    A package, obviously.  Just to forestall unnecessary replies.