EAGLE User Support (English) Linux printer font size too small in V500
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
  • Replies 6 replies
  • Subscribers 178 subscribers
  • Views 666 views
  • Users 0 members are here
Related

Linux printer font size too small in V500

autodeskguest
autodeskguest over 17 years ago

Hi All,

I've been running 4.16r2 Pro on my Gentoo box for years with no issues. I

recently upgraded to 5.00 and am trying it out on a simple board before I

go to 'full production status'. I've now run across two printing issues:

 

1) in the Print->Printer dialog box, the correct printer is shown in the

drop-down box. However, the 'Print Info:' text field below it shows the

current default CUPS printer, not the one in the dialog box. The drop-down

box printer (the Eagle default) is a B-Size printer; the default is my

office laser. Sure enough, all my printouts are letter-sized on my B-sized

printer. I believe there's a post in eagle.betatest that indicates this

might be a bug with QT and CUPS, and will be fixed in 5.1. Is this

confirmed, and any idea when 5.1 will be out?

 

2) The other issue I have is that no matter whether I print to a printer or

to PDF, the font sizes are tiny. Like, I need a magnifying glass to read

them. On screen the fonts are fine. A temporary workaround is to set the

fonts in Eagle to 'Always Vector Font' and 'Persistent', but then the PDFs

I create are not searchable. Is this another bug related to QT and CUPS and

the Eagle implementation thereof (no other app on this system has these

printing issues), or is there something else going on? I've tried

everything I've found on a search for 'font' in these groups: removed

~/.config/Trolltech.conf, checked DPI (95x95), tried various other fonts as

my default system font, etc. Nothing seems to work. Any ideas? Thanks.

 

 

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 17 years ago

    Klaus Schmidinger wrote:

     

    On 06/24/08 21:10, Robert Johnson wrote:

    ...

    2) The other issue I have is that no matter whether I print to a printer

    or to PDF, the font sizes are tiny. Like, I need a magnifying glass to

    read them. On screen the fonts are fine. A temporary workaround is to set

    the fonts in Eagle to 'Always Vector Font' and 'Persistent', but then the

    PDFs I create are not searchable. Is this another bug related to QT and

    CUPS and the Eagle implementation thereof (no other app on this system

    has these printing issues), or is there something else going on? I've

    tried everything I've found on a search for 'font' in these groups:

    removed ~/.config/Trolltech.conf, checked DPI (95x95), tried various

    other fonts as my default system font, etc. Nothing seems to work. Any

    ideas? Thanks.

     

    Since the problem happens in both PDFs and printouts, I doubt that

    this is a CUPS problem.

     

    My best guess is that it's a problem with your font setup (which

    probably triggers a bug in Qt - since other apps work fine).

     

    Printing works fine here on SUSE 10.3.

     

    Klaus Schmidinger

     

    I'm starting to lean towards a QT bug. If I place a fontconfig pattern

    command in my local .fonts.conf file to substitute courier with monospace,

    the text I've placed in the 'fixed' font starts printing OK, but the

    proportional spaced fonts still print really really small. Nothing I've

    tried so far seems to change that outcome. My google searches are coming up

    with some font-size errors with certain versions of the QT libraries. If

    you could, would you please tell me what the qtconfig help dialog gives for

    the QT version on SUSE 10.3? Gentoo seems to be at 4.3.3 currently. Thanks.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago in reply to autodeskguest

    Robert Johnson wrote:

     

    Klaus Schmidinger wrote:

     

    On 06/24/08 21:10, Robert Johnson wrote:

    ...

    2) The other issue I have is that no matter whether I print to a printer

    or to PDF, the font sizes are tiny. Like, I need a magnifying glass to

    read them. On screen the fonts are fine. A temporary workaround is to

    set the fonts in Eagle to 'Always Vector Font' and 'Persistent', but

    then the PDFs I create are not searchable. Is this another bug related

    to QT and CUPS and the Eagle implementation thereof (no other app on

    this system has these printing issues), or is there something else going

    on? I've tried everything I've found on a search for 'font' in these

    groups: removed ~/.config/Trolltech.conf, checked DPI (95x95), tried

    various other fonts as my default system font, etc. Nothing seems to

    work. Any ideas? Thanks.

     

    Since the problem happens in both PDFs and printouts, I doubt that

    this is a CUPS problem.

     

    My best guess is that it's a problem with your font setup (which

    probably triggers a bug in Qt - since other apps work fine).

     

    Printing works fine here on SUSE 10.3.

     

    Klaus Schmidinger

     

    I'm starting to lean towards a QT bug. If I place a fontconfig pattern

    command in my local .fonts.conf file to substitute courier with monospace,

    the text I've placed in the 'fixed' font starts printing OK, but the

    proportional spaced fonts still print really really small. Nothing I've

    tried so far seems to change that outcome. My google searches are coming

    up with some font-size errors with certain versions of the QT libraries.

    If you could, would you please tell me what the qtconfig help dialog gives

    for the QT version on SUSE 10.3? Gentoo seems to be at 4.3.3 currently.

    Thanks.

     

    Follow-up to my own post for the benefit of those who might ever come across

    this issue:

     

    I was able to fix this by turning off the scalable bitmap fonts. (In gentoo

    this is done using 'eselect fontconfig list' and then 'eselect fontconfig

    enable <#>' where # is the list entry for 'no-bitmaps.conf'.) I have no

    idea why this is only an issue with Eagle 5.0, or what combination of

    fonts / Qt / KDE / xorg triggers it, but I'm happy now image

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 17 years ago in reply to autodeskguest

    Robert Johnson wrote:

     

    Klaus Schmidinger wrote:

     

    On 06/24/08 21:10, Robert Johnson wrote:

    ...

    2) The other issue I have is that no matter whether I print to a printer

    or to PDF, the font sizes are tiny. Like, I need a magnifying glass to

    read them. On screen the fonts are fine. A temporary workaround is to

    set the fonts in Eagle to 'Always Vector Font' and 'Persistent', but

    then the PDFs I create are not searchable. Is this another bug related

    to QT and CUPS and the Eagle implementation thereof (no other app on

    this system has these printing issues), or is there something else going

    on? I've tried everything I've found on a search for 'font' in these

    groups: removed ~/.config/Trolltech.conf, checked DPI (95x95), tried

    various other fonts as my default system font, etc. Nothing seems to

    work. Any ideas? Thanks.

     

    Since the problem happens in both PDFs and printouts, I doubt that

    this is a CUPS problem.

     

    My best guess is that it's a problem with your font setup (which

    probably triggers a bug in Qt - since other apps work fine).

     

    Printing works fine here on SUSE 10.3.

     

    Klaus Schmidinger

     

    I'm starting to lean towards a QT bug. If I place a fontconfig pattern

    command in my local .fonts.conf file to substitute courier with monospace,

    the text I've placed in the 'fixed' font starts printing OK, but the

    proportional spaced fonts still print really really small. Nothing I've

    tried so far seems to change that outcome. My google searches are coming

    up with some font-size errors with certain versions of the QT libraries.

    If you could, would you please tell me what the qtconfig help dialog gives

    for the QT version on SUSE 10.3? Gentoo seems to be at 4.3.3 currently.

    Thanks.

     

    Follow-up to my own post for the benefit of those who might ever come across

    this issue:

     

    I was able to fix this by turning off the scalable bitmap fonts. (In gentoo

    this is done using 'eselect fontconfig list' and then 'eselect fontconfig

    enable <#>' where # is the list entry for 'no-bitmaps.conf'.) I have no

    idea why this is only an issue with Eagle 5.0, or what combination of

    fonts / Qt / KDE / xorg triggers it, but I'm happy now image