EAGLE User Support (English) Ratsnest problem in V5
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
  • Replies 1 reply
  • Subscribers 178 subscribers
  • Views 324 views
  • Users 0 members are here
Related

Ratsnest problem in V5

autodeskguest
autodeskguest over 17 years ago

I am having a bizarre problem.  When I ratsnest a board with copper polygon

pours on it, all of the polygons get processed and filled in, except those

with signal names GND and P5VA.   If I rename the polygon to some other name

it processes fine.   Previously, while working on the layout of the board, I

had hid the GND and P5VA signals using the RATSNEST ! GND P5VA command -

this worked great.  Later I cleared that by using the RATSNEST * and even

the RATSNEST GND  and RATSNEST P5VA commands.   These commands clearly make

the airwires appear for the signals named GND and P5VA, but the polygons

named GND or P5VA will still not process.   It does not matter which layer

the polygon is on.   I also deleted the polygons and redrew them and they

still will not process when I do a ratsnest.    I have no idea if the gerber

will be correct, but that really does not matter, the program has a problem

and I would really like to get my polygon pour processing back working.

Unless I am doing something stupid, this seems to be a bug related to hiding

of signals via the RATSNEST ! {signal name} command.

 

Regards

Darren

 

 

 

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • Richard_H
    Richard_H over 17 years ago

    Darren schrieb:

    I am having a bizarre problem.  When I ratsnest a board with copper polygon

    pours on it, all of the polygons get processed and filled in, except those

    with signal names GND and P5VA.   If I rename the polygon to some other name

    it processes fine.   Previously, while working on the layout of the board, I

    had hid the GND and P5VA signals using the RATSNEST ! GND P5VA command -

    this worked great.  Later I cleared that by using the RATSNEST * and even

    the RATSNEST GND  and RATSNEST P5VA commands.   These commands clearly make

    the airwires appear for the signals named GND and P5VA, but the polygons

    named GND or P5VA will still not process.   It does not matter which layer

    the polygon is on.   I also deleted the polygons and redrew them and they

    still will not process when I do a ratsnest.    I have no idea if the gerber

    will be correct, but that really does not matter, the program has a problem

    and I would really like to get my polygon pour processing back working.

    Unless I am doing something stupid, this seems to be a bug related to hiding

    of signals via the RATSNEST ! {signal name} command.

     

    Regards

    Darren

     

    Please try the following:

     

    RATSNEST *

     

    Check the setting:

    Options/Set/Misc  Ratsnest processes polygons.  Is it set?

     

    Do you have pads, vias, smds or wire bends inside the GND and

    P5VA polygons that belong to the polygon signal and are they

    reachable for the polygon (clearance, copper-dimension,

    resticted areas)?

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/faq.htm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Richard_H
    Richard_H over 17 years ago

    Darren schrieb:

    I am having a bizarre problem.  When I ratsnest a board with copper polygon

    pours on it, all of the polygons get processed and filled in, except those

    with signal names GND and P5VA.   If I rename the polygon to some other name

    it processes fine.   Previously, while working on the layout of the board, I

    had hid the GND and P5VA signals using the RATSNEST ! GND P5VA command -

    this worked great.  Later I cleared that by using the RATSNEST * and even

    the RATSNEST GND  and RATSNEST P5VA commands.   These commands clearly make

    the airwires appear for the signals named GND and P5VA, but the polygons

    named GND or P5VA will still not process.   It does not matter which layer

    the polygon is on.   I also deleted the polygons and redrew them and they

    still will not process when I do a ratsnest.    I have no idea if the gerber

    will be correct, but that really does not matter, the program has a problem

    and I would really like to get my polygon pour processing back working.

    Unless I am doing something stupid, this seems to be a bug related to hiding

    of signals via the RATSNEST ! {signal name} command.

     

    Regards

    Darren

     

    Please try the following:

     

    RATSNEST *

     

    Check the setting:

    Options/Set/Misc  Ratsnest processes polygons.  Is it set?

     

    Do you have pads, vias, smds or wire bends inside the GND and

    P5VA polygons that belong to the polygon signal and are they

    reachable for the polygon (clearance, copper-dimension,

    resticted areas)?

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/faq.htm