Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Running CAM Script to Get Gerber Files with Eagle SW
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 188 subscribers
  • Views 771 views
  • Users 0 members are here
Related

Running CAM Script to Get Gerber Files with Eagle SW

e14 Contributor
e14 Contributor over 15 years ago

I read that some type of script files (two of them) need to run after the Eagle CAD drawing are done. These need to be run to get CAM files and Gerber files in order to order pcbs. Is this true? Otherwise how are the CAM and Gerber files produced?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    On 2/12/2011 8:47 AM, Bronx68 wrote:

      I read that some type of script files (two of them) need to run after the Eagle CAD drawing are done. These need to be run to get CAM files and Gerber files in order to order pcbs. Is this true? Otherwise how are the CAM and Gerber files produced?

     

    Yes you need to run the CAM processor.   Eagle comes with some sample

    CAM job files....a good starting place for understanding how to setup

    the CAM processor to generate what you want.

     

    jiml

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    Are there existing script files that can be run to produce necessay files? Why are two script files required? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    On 2/12/2011 1:47 PM, Bronx68 wrote:

    Are there existing script files that can be run to produce necessay files? Why are two script files required?

     

    Those are the files Jim was referring to. One of the CAM jobs is used to

    generate gerber files, while the other is used to generate the required

    drill files. You could combine the two into one CAM job, but it's easier

    to keep track of things using the two seperate CAM jobs.

     

    You're going to use gerb274.cam and excellon.cam. See chap. 9 of the

    EAGLE manual for more information.

     

    hth,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    On 2/12/2011 1:47 PM, Bronx68 wrote:

    Are there existing script files that can be run to produce necessay files? Why are two script files required?

     

    Those are the files Jim was referring to. One of the CAM jobs is used to

    generate gerber files, while the other is used to generate the required

    drill files. You could combine the two into one CAM job, but it's easier

    to keep track of things using the two seperate CAM jobs.

     

    You're going to use gerb274.cam and excellon.cam. See chap. 9 of the

    EAGLE manual for more information.

     

    hth,

    Jorge Garcia