EAGLE User Support (English) Is there a ULP script for exporting pin names?
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
  • State Not Answered
  • Replies 6 replies
  • Subscribers 179 subscribers
  • Views 874 views
  • Users 0 members are here
  • ulp
Related

Is there a ULP script for exporting pin names?

Former Member
Former Member over 14 years ago

Hi,

 

I have a 48-pin microprocessor, and I'd like to make a bus for it in my schematic. Is there a way to export the pin names of the device from the library in a comma-delimited fashion?

 

Regards,

Tele

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 14 years ago

    Am 16.03.2011 17:32, schrieb Telemachus:

    Hi,

     

    I have a 48-pin microprocessor, and I'd like to make a bus for it in my schematic. Is there a way to export the pin names of the device from the library in a comma-delimited fashion?

     

    Regards,

    Tele

     

    EXPORT script ...

     

    HELP EXPORT (enter)

     

     

    Mit freundlichen Grüßen / Best regards

     

    Alfred Zaffran

    --

    _____________________________________________________________

    Alfred Zaffran              Support

    CadSoft Computer GmbH       Hotline:   08635-698930

    Pleidolfweg 15              FAX:       08635-698940

    84568 Pleiskirchen          eMail: <alf@cadsoft.de>

                                 Web:   <www.cadsoft.de>

    Registergericht: Amtsgericht Traunstein HRB 5573

    Geschäftsführer: Dipl.-Ing. Klaus Schmidinger, Bodo Badnowitz

    _____________________________________________________________

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • WestfW
    0 WestfW over 14 years ago in reply to Former Member

    I think the idea is that given a schematic that contains a BUS called "D0..15" and also a device that contains a symbol that has pins called "D0", "D1", ..., "D15", to somehow aid the connection of all those pins to that bus, rather than having to connect them one at a time.  Or at least get the names of all of the pins for use in a BUS command (so you can generate "bus A[0..31],B[0..31],RESET,CLOCK,IOSEL[0..1]"...

     

    That would be nice...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • WestfW
    0 WestfW over 14 years ago in reply to Former Member

    I think the idea is that given a schematic that contains a BUS called "D0..15" and also a device that contains a symbol that has pins called "D0", "D1", ..., "D15", to somehow aid the connection of all those pins to that bus, rather than having to connect them one at a time.  Or at least get the names of all of the pins for use in a BUS command (so you can generate "bus A[0..31],B[0..31],RESET,CLOCK,IOSEL[0..1]"...

     

    That would be nice...