EAGLE User Support (English) Copper pour using existing geometry
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
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 178 subscribers
  • Views 342 views
  • Users 0 members are here
  • existing
  • lines
  • geometry
  • pour
  • polygon
Related

Copper pour using existing geometry

Former Member
Former Member over 14 years ago

Hello.  I commonly make circuit boards that have very complex shapes.  The contours are usually created in our company's 3D CAD software.  Using VB.net, I was able to create a program that translates the board model into an Eagle script that, when run in a board window in Eagle, will draw the board for me.  This has been very useful.

 

However, I have a board that requires that the edges be wrapped with copper.  I have a supplier who will do it, but I can't seem to make Eagle generate the geometry I need.  If you look at the attached image, you will find my circuit board.  It's large with a single window cut out.  The small gap between the parallel paths is what I need filled with copper so that there is copper outlining the outer and inner edges of the board.  How can this be performed?

 

Thanks.

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • Former Member
    0 Former Member over 14 years ago

    gregd schrieb:

     

    Hello.  I commonly make circuit boards that have very complex shapes.

    The contours are usually created in our company's 3D CAD software.

    Using VB.net, I was able to create a program that translates the

    board model into an Eagle script that, when run in a board window in

    Eagle, will draw the board for me.  This has been very useful.

     

    However, I have a board that requires that the edges be wrapped with

    copper.  I have a supplier who will do it, but I can't seem to make

    Eagle generate the geometry I need.

     

    The only simple way I know of to solve that, is to draw additional

    (thicker) copper wires at the board outlines and NAME them accordingly.

    Your script generator could produce them as well - in case you don't

    need them, you can easily delete (parts of) them later in the board.

    Note that the DRC will complain about this (ignore/acknowledge these

    errors).

     

    If you look at the attached image, you will find my circuit board.

     

    There is no attached image - at least not anywhere outside of that #@$%

    forum at element14. You might consider using direct newsgroup access or

    having a look at the other web based interface at eaglecentral.ca (which

    at least is far better than that of element14).

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • Former Member
    0 Former Member over 14 years ago

    gregd schrieb:

     

    Hello.  I commonly make circuit boards that have very complex shapes.

    The contours are usually created in our company's 3D CAD software.

    Using VB.net, I was able to create a program that translates the

    board model into an Eagle script that, when run in a board window in

    Eagle, will draw the board for me.  This has been very useful.

     

    However, I have a board that requires that the edges be wrapped with

    copper.  I have a supplier who will do it, but I can't seem to make

    Eagle generate the geometry I need.

     

    The only simple way I know of to solve that, is to draw additional

    (thicker) copper wires at the board outlines and NAME them accordingly.

    Your script generator could produce them as well - in case you don't

    need them, you can easily delete (parts of) them later in the board.

    Note that the DRC will complain about this (ignore/acknowledge these

    errors).

     

    If you look at the attached image, you will find my circuit board.

     

    There is no attached image - at least not anywhere outside of that #@$%

    forum at element14. You might consider using direct newsgroup access or

    having a look at the other web based interface at eaglecentral.ca (which

    at least is far better than that of element14).

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • Former Member
    0 Former Member over 14 years ago in reply to Former Member

    After thinking about it a bit more, I did just that.  Thanks for confirming my approach.

     

    Most of the region where I needed the copper was uniform width, so that solution worked well for those areas.  I also had a few spots where I needed something a bit narrower, but I generated the appropriate geometry given the offset I was going to apply, and that worked great.

     

    I don't know about the image attachment.  The Cadsoft website suggested element14, so I assumed it would host properly.  I know for next time.

     

    Thanks again.