EAGLE User Support (English) Highlight Airwires
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
  • State Not Answered
  • Replies 5 replies
  • Subscribers 179 subscribers
  • Views 640 views
  • Users 0 members are here
Related

Highlight Airwires

tmartin
tmartin over 14 years ago

What is the command or process to locate very small airwires?  Ratsnest is identifying one airwire; I can't see it (I have turned off the trace layers in an effort to aid in identifying its location).

  • Sign in to reply
  • Cancel

Top Replies

  • Former Member
    Former Member over 14 years ago +1
    Am 11.05.2011 21:05, schrieb tmartin: What is the command or process to locate very small airwires? > Ratsnest is identifying one airwire; I can't see it (I have turned > off the trace layers in an effort…
Parents
  • Former Member
    0 Former Member over 14 years ago

    Am 11.05.2011 21:05, schrieb tmartin:

      What is the command or process to locate very small airwires?

    >  Ratsnest is identifying one airwire; I can't see it (I have turned

    > off the trace layers in an effort to aid in identifying its location).

     

    SET CATCH_FACTOR 0; ROUTE  (enter) click in board ...

     

    or set

     

    Options - Set - Misc - Catch factor = 0

     

    ROUTE click in board ...

     

     

    please read

    HELP SET (enter)

    HELP ROUTE (enter)

     

     

    Mit freundlichen Grüßen / Best regards

     

    Alfred Zaffran

    --

    _____________________________________________________________

    Alfred Zaffran              Support

    CadSoft Computer GmbH       Hotline:   08635-698930

    Pleidolfweg 15              FAX:       08635-698940

    84568 Pleiskirchen          eMail: <alf@cadsoft.de>

                                 Web:   <www.cadsoft.de>

    Registergericht: Amtsgericht Traunstein HRB 5573

    Geschäftsführer: Dipl.-Ing. Klaus Schmidinger, Bodo Badnowitz

    _____________________________________________________________

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tmartin
    0 tmartin over 14 years ago in reply to Former Member

    Thanks Alf_Z.  Found the airwire. The next trick is to find the location to mark the question as answered.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • tmartin
    0 tmartin over 14 years ago in reply to Former Member

    Thanks Alf_Z.  Found the airwire. The next trick is to find the location to mark the question as answered.