EAGLE User Support (English) DRC and VIAs
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
  • State Not Answered
  • Replies 2 replies
  • Subscribers 178 subscribers
  • Views 358 views
  • Users 0 members are here
  • eagle
  • drc
  • via
Related

DRC and VIAs

Former Member
Former Member over 14 years ago

I am using Eagle Pro 5.11 to place 6mil vias with 12 mil pads onto a GND polygon.  The vias are named GND as well.  This works well.

 

However, DRC complains about a DRILL CLEARANCE issue.  I have tried reducing the DRC-CLEARANCE-VIA-VIA and VIA-SMD down to 1mil to no avail.

 

 

Is there another location where I should change the DRC rules for drill clearances?

 

Billy

  • Sign in to reply
  • Cancel
  • Former Member
    0 Former Member over 14 years ago

    On 5/16/2011 11:31 AM, Billy Coleman wrote:

    I am using Eagle Pro 5.11 to place 6mil vias with 12 mil pads onto a GND polygon.  The vias are named GND as well.  This works well.

     

    However, DRC complains about a DRILL CLEARANCE issue.  I have tried reducing the DRC-CLEARANCE-VIA-VIA and VIA-SMD down to 1mil to no avail.

     

    >

     

    Is there another location where I should change the DRC rules for drill clearances?

     

    Billy

     

    have you tried reducing it to zero?

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 14 years ago

    Am 16.05.2011 20:31, schrieb Billy Coleman:

    I am using Eagle Pro 5.11 to place 6mil vias with 12 mil pads onto a GND polygon.

    > The vias are named GND as well.  This works well.

     

    However, DRC complains about a DRILL CLEARANCE issue.  I have tried reducing the

    > DRC-CLEARANCE-VIA-VIA and VIA-SMD down to 1mil to no avail.

     

    This is the copper-clearance (restring)!

     

     

     

    Is there another location where I should change the DRC rules for drill clearances?

     

    DRC -- Distance -- Drill/Hole ...

    Check more at one drill (Via) on same coordinate, you can delete a VIA

    by RIPUP and click on center of the via.

     

    HELP RIPUP

    HELP RATSNEST

     

     

     

    Mit freundlichen Grüßen / Best regards

     

    Alfred Zaffran

    --

    _____________________________________________________________

    Alfred Zaffran              Support

    CadSoft Computer GmbH       Hotline:   08635-698930

    Pleidolfweg 15              FAX:       08635-698940

    84568 Pleiskirchen          eMail: <alf@cadsoft.de>

                                 Web:   <www.cadsoft.de>

    Registergericht: Amtsgericht Traunstein HRB 5573

    Geschäftsführer: Dipl.-Ing. Klaus Schmidinger, Bodo Badnowitz

    _____________________________________________________________