EAGLE User Support (English) How to put a clearance-distance border around vias without Stop Mask errors?
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
  • State Not Answered
  • Replies 0 replies
  • Subscribers 177 subscribers
  • Views 118 views
  • Users 0 members are here
  • board
  • eagle
  • drc
  • question
Related

How to put a clearance-distance border around vias without Stop Mask errors?

gbulmeruk
gbulmeruk over 14 years ago

I'd like a border around vias to show the clearance distance from the edges of the via. I think this helps me hand route boards.

For example, a 40mil diameter via with a 10mil clearance would have a 60mil diameter border. I'd expect it to work for all shapes of via.

 

The only way I've found to do it is set the clearance as the min/max for a stop mask in the Design Rule dialogue.

 

I don't like that as a solution because all of the component names (which I like to have on) generate hundreds of Stop Mask errors which is a distraction, and might hide useful error information (which is even more distracting because I have to manually check the error dialogue, or approve them whenever I move a component).

 

Is there a way to get the visual effect without getting any Name/Stop Mask errors?

It doesn't need to be a stop mask, it is the visual feedback which I am looking for.

I'm happy to use the Stop Mask if I can switch off the Stop Mask errors generated by component names.

 

I would like the clearance-distance border around pads, so maybe defeating the 'Names on Stop Mask' errors might be sufficient.

 

Then I'd like a clearance distance border around tracks too, please image