Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Error  Only INPUT pins on net ...
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 189 subscribers
  • Views 4119 views
  • Users 0 members are here
Related

Error  Only INPUT pins on net ...

e14 Contributor
e14 Contributor over 15 years ago

Hello,

 

I have the error Only INPUT pins on net ... twice: for V- IC1A and V- IC1B

 

Honnestly I have been looking for solutions for 3 days and nothing.

 

These errors drive me crazy. If I someone has a solution ...

 

 

Thx

 

Here is my schematic:

http://imageshack.us/photo/my-images/14/captureyq.jpg/

  • Sign in to reply
  • Cancel
  • trackerfx
    0 trackerfx over 5 years ago

    I realize that this is an old post, but since no one has answered it I'll give it a whack.

     

    By default when you create a part in Eagle pins are assigned with the direction field equal to 'IO'. As such, Eagle will not throw 'Only INPUT pins on net' errors, as it can be either input or output. However, if you change the pin direction to 'input' and there are no pins on the same net that are assigned as an output or IO Eagle will give you an error. Likewise, if the only pins assigned to a net are outputs Eagle will throw a 'Only OUTPUT pins on net' error.

     

    Moral of the story: You cannot have only inputs (or only outputs) on a net. If you're getting this error check the direction field of the pins on that net. Make sure you have at least one input and one output or IO.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    Ahxl <communitymanager@premierfarnell.com> wrote:

    Hello,

     

    I have the error Only INPUT pins on net ... twice: for V- IC1A and V- IC1B

     

    Honnestly I have been looking for solutions for 3 days and nothing.

     

    These errors drive me crazy. If I someone has a solution ...

     

    The easiest way ti check if you REALLY have made a connection to a symbol

    is to try moving the symbol around a bit. If the connections follow, you

    are connected.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    Ahxl schrieb:

     

    I have the error Only INPUT pins on net ... twice: for V- IC1A and V- IC1B

     

    If you look a little further, you can see that there also is only one

    pin connected to these particular nets. (And there are some more

    warnings of that kind.)

     

    Obviously, you didn't /really/ connect the nets to the pins as intended.

    Maybe you used WIRE instead of NET, maybe you tried to MOVE net ends to

    pins, maybe you didn't use correct (i.e. matching) grid settings.

     

    Try SHOW on the nets N$1 and N$4 to see what highlights. If a pin is

    connected to a net, it will highlight too.

     

    Correct your connections, then these errors will disappear.

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer