EAGLE User Support (English) Board Editing - Feature Missing
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
  • Replies 2 replies
  • Subscribers 178 subscribers
  • Views 250 views
  • Users 0 members are here
Related

Board Editing - Feature Missing

autodeskguest
autodeskguest over 17 years ago

Hi,

 

Using Ubuntu Hardy.

 

In version 4.x when manually routing the board when I pressed the left mouse

button it would grab the closest available unrouted net.

 

However in 5.1 it only beeps. 4.x would only beep if there were no unrouted

nets.

 

The previous feature was a great help because sometimes there are nets that

need top be routed but are hard to see. Without the feature it is possible

to miss a net.

 

Thanks

 

Grahame Jordan

 

 

  • Sign in to reply
  • Cancel
  • Richard_H
    Richard_H over 17 years ago

    Grahame Jordan schrieb:

    Hi,

     

    Using Ubuntu Hardy.

     

    In version 4.x when manually routing the board when I pressed the left mouse

    button it would grab the closest available unrouted net.

     

    However in 5.1 it only beeps. 4.x would only beep if there were no unrouted

    nets.

     

    The previous feature was a great help because sometimes there are nets that

    need top be routed but are hard to see. Without the feature it is possible

    to miss a net.

     

    Thanks

     

    Grahame Jordan

     

     

    Please check Options/Set/Misc

     

    Catch factor:

    Within this radius a mouse click can reach objects. Set the value

    to 0 in order to switch this limitation off. EAGLE behaves now

    as in previous versions: You can reach even objects that are placed

    far beyond the area of the current display window. Default: 5% of

    the height of the current display window.

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/faq.htm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 17 years ago

    Hi Richard,

     

    Thanks, That works just great

     

    Cheers

     

    Grahame Jordan

     

     

    Richard Hammerl wrote:

     

    Grahame Jordan schrieb:

    Hi,

     

    Using Ubuntu Hardy.

     

    In version 4.x when manually routing the board when I pressed the left

    mouse button it would grab the closest available unrouted net.

     

    However in 5.1 it only beeps. 4.x would only beep if there were no

    unrouted nets.

     

    The previous feature was a great help because sometimes there are nets

    that need top be routed but are hard to see. Without the feature it is

    possible to miss a net.

     

    Thanks

     

    Grahame Jordan

     

     

    Please check Options/Set/Misc

     

    Catch factor:

    Within this radius a mouse click can reach objects. Set the value

    to 0 in order to switch this limitation off. EAGLE behaves now

    as in previous versions: You can reach even objects that are placed

    far beyond the area of the current display window. Default: 5% of

    the height of the current display window.