Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Importing library script failing
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 184 subscribers
  • Views 265 views
  • Users 0 members are here
Related

Importing library script failing

zainka
zainka over 14 years ago

A custom library was exported using the export command, then some of the symbol Text elements where edited and saved. Then I tried to run the script in a new library to import all sym, pac and devices. Then first it imports all the symbols without errors, then Eagle tries to import the packages into the symbol editor (I can see it is drawing the packages on top of the last symbol imported), but it fails because several of the layers used in Pacacke editor is not available in the symbol editor. How to solve this??? Why does a script generated by Eagle fail in Eagle? I tried to generate the script once more and the run it in new library without changing anything, but same error happens.

 

 

Thanks in advance

Vidar (Z)

  • Sign in to reply
  • Cancel
  • Former Member
    0 Former Member over 14 years ago

    Am 07.08.2011 23:26, schrieb vidar vidnes:

      A custom library was exported using the export command, then some of the symbol Text elements where edited and saved. Then I tried to run the script in a new library to import all sym, pac and devices. Then first it imports all the symbols without errors, then Eagle tries to import the packages into the symbol editor (I can see it is drawing the packages on top of the last symbol imported), but it fails because several of the layers used in Pacacke editor is not available in the symbol editor. How to solve this??? Why does a script generated by Eagle fail in Eagle? I tried to generate the script once more and the run it in new library without changing anything, but same error happens.

     

    >

    Thanks in advance

    Vidar (Z)

     

     

    I suppose that there was a fault in the library anyway. I do a lot of

    in- and exporting of libraries and never had any trouble. Maybe you can

    place a zip-copy of that library here so one may have a look into it.

    (AFAIK the limit here is 50 kB, if it is larger send it to me via PM or

    ask cadsoft to look into it).

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer