EAGLE User Support (English) Does Eagle have the capability to produce ODB++ files?
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
  • State Suggested Answer
  • Replies 11 replies
  • Answers 1 answer
  • Subscribers 184 subscribers
  • Views 4363 views
  • Users 0 members are here
Related

Does Eagle have the capability to produce ODB++ files?

Former Member
Former Member over 14 years ago

Can I produce an ODB++ file  with Eagle ?

  • Sign in to reply
  • Cancel

Top Replies

  • autodeskguest
    autodeskguest over 10 years ago in reply to gadget.iom +1
    Hi Guys, Nothing yet, but we hope to have something soon. Best Regards, Jorge Garcia
Parents
  • Former Member
    0 Former Member over 14 years ago

    On 8/24/2011 10:54 AM, Joe Adler wrote:

    Can I produce an ODB++ file  with Eagle ?

     

     

    Hi Joe,

     

    I'm afraid not. The ODB++ is a closed standard and requires an NDA to

    use. Since we would likely implement the format using a ULP which is a

    simple text file, i'm sure you could see why that wouldn't have worked

    out so well.

     

    The format could've been implemented internal to EAGLE, however the

    developers decided not to support the format. You'd have to ask them why.

     

    hth,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • amigabill
    0 amigabill over 14 years ago in reply to Former Member

    Perhaps when Eagle changes over to the XML data format and its

    description as mentioned in another topic, someone can NDA the format

    and make a closed-source translator. Too bad an Ulp wouldn't be allowed

    due to odb++ licensing. :/ If a similar someone could NDA the existing

    binary Eagle data formats perhaps a similar closed-source translator

    program could do that as well, but it sounds like life for such a

    someone will be easier in a few months.

     

     

     

    Jorge Garcia wrote:

    On 8/24/2011 10:54 AM, Joe Adler wrote:

    >> Can I produce an ODB++ file  with Eagle ?

    >>

     

    Hi Joe,

     

    I'm afraid not. The ODB++ is a closed standard and requires an NDA to

    use. Since we would likely implement the format using a ULP which is a

    simple text file, i'm sure you could see why that wouldn't have worked

    out so well.

     

    The format could've been implemented internal to EAGLE, however the

    developers decided not to support the format. You'd have to ask them why.

     

    hth,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • amigabill
    0 amigabill over 14 years ago in reply to Former Member

    Perhaps when Eagle changes over to the XML data format and its

    description as mentioned in another topic, someone can NDA the format

    and make a closed-source translator. Too bad an Ulp wouldn't be allowed

    due to odb++ licensing. :/ If a similar someone could NDA the existing

    binary Eagle data formats perhaps a similar closed-source translator

    program could do that as well, but it sounds like life for such a

    someone will be easier in a few months.

     

     

     

    Jorge Garcia wrote:

    On 8/24/2011 10:54 AM, Joe Adler wrote:

    >> Can I produce an ODB++ file  with Eagle ?

    >>

     

    Hi Joe,

     

    I'm afraid not. The ODB++ is a closed standard and requires an NDA to

    use. Since we would likely implement the format using a ULP which is a

    simple text file, i'm sure you could see why that wouldn't have worked

    out so well.

     

    The format could've been implemented internal to EAGLE, however the

    developers decided not to support the format. You'd have to ask them why.

     

    hth,

    Jorge Garcia