Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) How to solder a 2-layer board with no busses?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 188 subscribers
  • Views 571 views
  • Users 0 members are here
Related

How to solder a 2-layer board with no busses?

e14 Contributor
e14 Contributor over 15 years ago

Hi everyone,

 

I'm a newby and this is my fist post here.

I have a question about layers but can't find the answer on the forum here.

 

The problem case:

 

I want to make a PCB of two layers, 1 and 16.

Because this PCB is etched by myself, the pads on both sides are not initally connected to eachother (with busses is it called?)

Using the autorouter of Eagle, it will create tracks on both sides of the board.

But if I want to mount, let say, an IC socket, I can't reach the socket pins on the top side of the board with my solder iron.

This pin has to be soldered, because some track is connected to that pin.

 

This problem can be solved in two ways I think.

1. Try to create a 1-layer board.

2. Use vias right next to the pads, so that you can create the needed connection from top to bottom.

 

Both sollutions are not realy nice.

 

Are the ways to setup the autorouter to get what I want?

I assume there must be more poeple avout here that are facing the same problem...

 

Hope to hear tou soon.

 

PeterZ

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    Peter Zomer <communitymanager@premierfarnell.com> wrote:

    Hi everyone,

     

    I'm a newby and this is my fist post here.

    I have a question about layers but can't find the answer on the forum here.

     

    The problem case:

     

    I want to make a PCB of two layers, 1 and 16.

    Because this PCB is etched by myself, the pads on both sides are not

    initally connected to eachother (with busses is it called?)

    Using the autorouter of Eagle, it will create tracks on both sides of the board.

    But if I want to mount, let say, an IC socket, I can't reach the socket

    pins on the top side of the board with my solder iron.

    This pin has to be soldered, because some track is connected to that pin.

     

    This problem can be solved in two ways I think.

    1. Try to create a 1-layer board.

    2. Use vias right next to the pads, so that you can create the needed

    connection from top to bottom.

     

    Both sollutions are not realy nice.

     

    Are the ways to setup the autorouter to get what I want?

    I assume there must be more poeple avout here that are facing the same problem...

     

    The easy solution is to NOT use through hole ICs. Soldering smd's by hand

    is easier than you think. I even prefer it over through hole. Many

    connectors also come as smd.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 15 years ago

    Peter Zomer <communitymanager@premierfarnell.com> wrote:

    Hi everyone,

     

    I'm a newby and this is my fist post here.

    I have a question about layers but can't find the answer on the forum here.

     

    The problem case:

     

    I want to make a PCB of two layers, 1 and 16.

    Because this PCB is etched by myself, the pads on both sides are not

    initally connected to eachother (with busses is it called?)

    Using the autorouter of Eagle, it will create tracks on both sides of the board.

    But if I want to mount, let say, an IC socket, I can't reach the socket

    pins on the top side of the board with my solder iron.

    This pin has to be soldered, because some track is connected to that pin.

     

    This problem can be solved in two ways I think.

    1. Try to create a 1-layer board.

    2. Use vias right next to the pads, so that you can create the needed

    connection from top to bottom.

     

    Both sollutions are not realy nice.

     

    Are the ways to setup the autorouter to get what I want?

    I assume there must be more poeple avout here that are facing the same problem...

     

    The easy solution is to NOT use through hole ICs. Soldering smd's by hand

    is easier than you think. I even prefer it over through hole. Many

    connectors also come as smd.