Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) How to solder a 2-layer board with no busses?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 188 subscribers
  • Views 567 views
  • Users 0 members are here
Related

How to solder a 2-layer board with no busses?

e14 Contributor
e14 Contributor over 15 years ago

Hi everyone,

 

I'm a newby and this is my fist post here.

I have a question about layers but can't find the answer on the forum here.

 

The problem case:

 

I want to make a PCB of two layers, 1 and 16.

Because this PCB is etched by myself, the pads on both sides are not initally connected to eachother (with busses is it called?)

Using the autorouter of Eagle, it will create tracks on both sides of the board.

But if I want to mount, let say, an IC socket, I can't reach the socket pins on the top side of the board with my solder iron.

This pin has to be soldered, because some track is connected to that pin.

 

This problem can be solved in two ways I think.

1. Try to create a 1-layer board.

2. Use vias right next to the pads, so that you can create the needed connection from top to bottom.

 

Both sollutions are not realy nice.

 

Are the ways to setup the autorouter to get what I want?

I assume there must be more poeple avout here that are facing the same problem...

 

Hope to hear tou soon.

 

PeterZ

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Am 04.09.2011 20:44, schrieb Peter Zomer:

    Because this PCB is etched by myself, the pads on both sides are not initally connected to eachother (with busses is it called?)

     

    A connection between board layers is called 'via'. There is even an

    EAGLE command available with the same name and for exactly that purpose.

    A 'bus' only exists in the schematics and is sort of a container for

    several nets belonging together, e.g. DATA[0], DATA[1], DATA[2],...

     

    But if I want to mount, let say, an IC socket, I can't reach the socket pins on the top side of the board with my solder iron.

     

    That depends on the sockets you are using. Since the majority of our

    boards is also not 'through-plated' (and has no connections between

    layers), we are using so-called 'carrier sockets': These are just single

    pins without plastic frame that are held together by a brass carrier.

    After soldering (which works well on both sides), the carrier is

    removed. That is the easiest solution, but those carrier sockets are not

    exactly cheap...

     

    2. Use vias right next to the pads, so that you can create the needed connection from top to bottom.

     

    In order to do that, you can create rectangles around the IC pads in the

    layer 'tRestrict' to prevent EAGLE from connecting these pads to the top

    layer. Instead, vias will be automatically placed somewhere else.

     

    Are the ways to setup the autorouter to get what I want?

     

    Your problem doesn't only concern ICs, but also other components like

    trimmers, large capacitors, etc.: You wouldn't want to have vias placed

    BELOW, e.g., a large capacitor. Creating all tRestrict areas to prevent

    the autorouter from connecting things to the top there is quite some

    work, if you don't want single-sided boards. Therefore, it is probably a

    good idea NOT to use the autorouter at all. It doesn't create nice

    boards, anyway. If you need a purely digital board, the autorouter is

    OK, but I advise against it for analog boards - the results look too

    strange...

     

    Andreas Weidner

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Am 04.09.2011 20:44, schrieb Peter Zomer:

    Because this PCB is etched by myself, the pads on both sides are not initally connected to eachother (with busses is it called?)

     

    A connection between board layers is called 'via'. There is even an

    EAGLE command available with the same name and for exactly that purpose.

    A 'bus' only exists in the schematics and is sort of a container for

    several nets belonging together, e.g. DATA[0], DATA[1], DATA[2],...

     

    But if I want to mount, let say, an IC socket, I can't reach the socket pins on the top side of the board with my solder iron.

     

    That depends on the sockets you are using. Since the majority of our

    boards is also not 'through-plated' (and has no connections between

    layers), we are using so-called 'carrier sockets': These are just single

    pins without plastic frame that are held together by a brass carrier.

    After soldering (which works well on both sides), the carrier is

    removed. That is the easiest solution, but those carrier sockets are not

    exactly cheap...

     

    2. Use vias right next to the pads, so that you can create the needed connection from top to bottom.

     

    In order to do that, you can create rectangles around the IC pads in the

    layer 'tRestrict' to prevent EAGLE from connecting these pads to the top

    layer. Instead, vias will be automatically placed somewhere else.

     

    Are the ways to setup the autorouter to get what I want?

     

    Your problem doesn't only concern ICs, but also other components like

    trimmers, large capacitors, etc.: You wouldn't want to have vias placed

    BELOW, e.g., a large capacitor. Creating all tRestrict areas to prevent

    the autorouter from connecting things to the top there is quite some

    work, if you don't want single-sided boards. Therefore, it is probably a

    good idea NOT to use the autorouter at all. It doesn't create nice

    boards, anyway. If you need a purely digital board, the autorouter is

    OK, but I advise against it for analog boards - the results look too

    strange...

     

    Andreas Weidner