Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) SOT223 and pins
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 187 subscribers
  • Views 1120 views
  • Users 0 members are here
Related

SOT223 and pins

autodeskguest
autodeskguest over 18 years ago

Hi,

 

I know we can assign a pin to two or more pads. Sometimes this is

necessary, indeed.

 

For example a SOT223 has four pads and usually the middle is connected

to the exposed one.

 

In the schematic makes no sense to show two pins: let's think a mosfet

with two drains....

 

What do you do to make the schematic readable and the layout correct

(e.g. both pads connected) ?

 

Thanks

Marco / iw2nzm

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 18 years ago

    Marco Trapanese wrote:

    For example a SOT223 has four pads and usually the middle is connected

    to the exposed one.

     

    In the schematic makes no sense to show two pins: let's think a mosfet

    with two drains....

     

    Sometimes it is useful for making efficient routing and use the drain

    pins to jump.

     

    But in other cases i agree with opinions in this thread...

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 18 years ago

    Marco Trapanese wrote:

    Marco Trapanese ha scritto:

     

    Clench your teeth, put the multiple pins in the symbol, and with

    time you'll get used to it....

     

    Furthermore there is another bad thing. Many voltage regulator share

    the same packages. So it would be nice to have only one device with

    several variants, one for each package version.

     

    Simply it is not possible. TO92 or TO220 have three pins, SOT223 has

    four pins (GND pin and GND tab) so they can't live togheter. Ok, I

    need two devices. But let me say it's a "bit" trivial...

     

    I agree with you on this one.  It is unfortunate that you end up having to

    make separate devices for the same part in different packages.  I wish some

    bright guy at CadSoft would think of a way around this.

     

    Maybe an "optional" setting for symbol pins?  That way a symbol pin might or

    might not be used when connecting it to a package in a device.  I wonder

    what kind of problems that might lead to....

     

    --

    Bert Menkveld

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 18 years ago

    Marco Trapanese ha scritto:

     

    Clench your teeth, put the multiple pins in the symbol, and with time

    you'll get used to it....

     

     

    Furthermore there is another bad thing. Many voltage regulator share the

    same packages. So it would be nice to have only one device with several

    variants, one for each package version.

     

    Simply it is not possible. TO92 or TO220 have three pins, SOT223 has

    four pins (GND pin and GND tab) so they can't live togheter. Ok, I need

    two devices. But let me say it's a "bit" trivial...

     

    Marco / iw2nzm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 18 years ago

    Bert Menkveld ha scritto:

     

    Clench your teeth, put the multiple pins in the symbol, and with time you'll

    get used to it....

     

     

    I won't get used to it..l It's a lack of the CAD. I've never seen a

    schematic like that. It should show the actual function of the pin

    rather the physical connection.

     

    Marco / iw2nzm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 18 years ago

    Marco Trapanese wrote:

    Hi,

     

    I know we can assign a pin to two or more pads. Sometimes this is

    necessary, indeed.

     

    For example a SOT223 has four pads and usually the middle is connected

    to the exposed one.

     

    In the schematic makes no sense to show two pins: let's think a mosfet

    with two drains....

     

    Well, that is exactly what I end up doing.  Although it seems ugly at first,

    it actually makes good sense.  For example, I have a MOSFET on a schematic

    in front of me right now.  It's in a 4-pin DIP package, and looking at my

    schematic I can see that the drain is connected to pins 1 and 2, because

    both of those pins are shown on the symbol.  If the schematic symbol only

    had one drain pin shown, then I wouldn't be able to see both those pin

    numbers, and I might have to pull out the datasheet to figure out what that

    unknown pin is for.

     

    What do you do to make the schematic readable and the layout correct

    (e.g. both pads connected) ?

     

    Clench your teeth, put the multiple pins in the symbol, and with time you'll

    get used to it....

     

    Thanks

    Marco / iw2nzm

     

    --

    Bert Menkveld