EAGLE User Support (English) Copper pour doesn't fill anymore
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
  • Replies 6 replies
  • Subscribers 180 subscribers
  • Views 2194 views
  • Users 0 members are here
Related

Copper pour doesn't fill anymore

autodeskguest
autodeskguest over 17 years ago

Hello,

 

I'm working on a board file since several time. I don't know what I did

but now copper pour (polygons) doesn't fill anymore. They shows only the

edge.

 

I closed and restarted Eagle but no way.

 

Do you have any idea what I did? I'm not a newbie about this topic but

this time I can't handle the situation...

 

Thanks

Marco / iw2nzm

 

  • Sign in to reply
  • Cancel
Parents
  • Richard_H
    Richard_H over 17 years ago

    Marco Trapanese schrieb:

    Marco Trapanese ha scritto:

     

    I'm working on a board file since several time. I don't know what I

    did but now copper pour (polygons) doesn't fill anymore. They shows

    only the edge.

     

    Update:

     

    the area is filled until I rename the polygon as 'gnd'. Since that it

    will remain empty, even if I change again the name.

     

    What could lead to this?

     

    Marco / iw2nzm

     

     

    The polygon name determines the signal it will be connected to.

    GND is available inside the polygon contour, so the polygon is

    filled. If you choose another signal name for the polygon and

    there are no objects that belong to this signal inside the

    polygon it can't be connected to anything and it won't be

    calculated. Provided the option Orphans is set OFF, which is

    default.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/faq.htm

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Richard_H
    Richard_H over 17 years ago

    Marco Trapanese schrieb:

    Marco Trapanese ha scritto:

     

    I'm working on a board file since several time. I don't know what I

    did but now copper pour (polygons) doesn't fill anymore. They shows

    only the edge.

     

    Update:

     

    the area is filled until I rename the polygon as 'gnd'. Since that it

    will remain empty, even if I change again the name.

     

    What could lead to this?

     

    Marco / iw2nzm

     

     

    The polygon name determines the signal it will be connected to.

    GND is available inside the polygon contour, so the polygon is

    filled. If you choose another signal name for the polygon and

    there are no objects that belong to this signal inside the

    polygon it can't be connected to anything and it won't be

    calculated. Provided the option Orphans is set OFF, which is

    default.

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/faq.htm