Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Filled vias
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 189 subscribers
  • Views 1546 views
  • Users 0 members are here
Related

Filled vias

e14 Contributor
e14 Contributor over 14 years ago

HI,

 

I am new to this and am only using eagle to design boards/substrates for microeletronic packages. I would prefer to do it in 3D cad, but PCB suppliers prefere to have gerber file...

 

  1. How do I create a plugged/filled vias with a pad on both top and bottom?
  2. Can I have different size and shape pads on top and bottom when creating a via?
  3. How do I create a substrate with a cavity?
  • Sign in to reply
  • Cancel
Parents
  • jeromeabcpcb
    0 jeromeabcpcb over 14 years ago

    "Magnus Adelmor"  a écrit dans le message de groupe de discussion :

    1819182079.8511317738586354.JavaMail.jive@flmspu-csapp-02.premierfarnell.com...

     

    HI,

     

    I am new to this and am only using eagle to design boards/substrates for

    microeletronic packages. I would prefer to do it in 3D cad, but PCB

    suppliers prefere to have gerber file...

     

    1. How do I create a plugged/filled vias with a pad on both top and bottom?

     

    2. Can I have different size and shape pads on top and bottom when creating

    a via?

     

    3. How do I create a substrate with a cavity?

     

     

     

     

    Hello Magnus,

     

    Conventional PCBs are pretty different from microelectronics technologies. I

    am not aware of any manufacturer that offer plugged vias nor cavity, so you

    will have to trick them.

    For the cavity you could use a stack of three thin PCB. The issue will be to

    interconnect them. Depending on the number of connection, you could use

    through hole conenctors, or some bondings.

     

    As you probably have a limited number of traces you could just draw them

    with rectangles/lines on top & bottom layers directly, without using the

    traces. This way you have perfect control on spacing and width.

    Avoid Eagle vias and draw your pads with any shape. Just add a drill in the

    middle.

     

    Do you have a good reason for a filled vias ? Maybe you can use very narrow

    drills instead ? Vias typically have similar thickness as the copper layers.

     

    Jerome

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to jeromeabcpcb

    Hi Jerome,

     

    Thanks for your help.

     

    We have a substrate manufacturer who does plugged vias. We will perform ball bondning on the pad, therefore we need the via filled.

     

    Your description on how to make cavities is what we would like to do. But how do I make make a cut-out in the top pcb in order to create a cavity? Can I design these three pcb's as a stacked design and only create a cut out in one of the pcb's?

     

    If I do not use Eagle's via, how do I tell the manufacturer that the small hole should be a via, a filled via? Besides being new to Eagle, I have a lack of understanding regarding gerber files and drill files...

     

    Mags

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    On 10/05/2011 03:56 PM, Magnus Adelmor wrote:

    Hi Jerome,

     

    Thanks for your help.

     

    We have a substrate manufacturer who does plugged vias. We will

    perform ball bondning on the pad, therefore we need the via filled.

     

    Your description on how to make cavities is what we would like to do.

    But how do I make make a cut-out in the top pcb in order to create a

    cavity? Can I design these three pcb's as a stacked design and only

    create a cut out in one of the pcb's?

     

    I believe what you're looking for is called a "blind via", which is a

    via that begins on one surface of the board, but does not penetrate

    through to the other side - it stops on an inner layer.

     

    Blind vias can be setup in eagle's DRC dialog box.  Since I have never

    used blind vias, I can not purport to know how to set them up.  The

    DRC->Layers tab provides an example with which you can start.

     

    Enjoy,

        - Chuck

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    On 10/05/2011 03:56 PM, Magnus Adelmor wrote:

    Hi Jerome,

     

    Thanks for your help.

     

    We have a substrate manufacturer who does plugged vias. We will

    perform ball bondning on the pad, therefore we need the via filled.

     

    Your description on how to make cavities is what we would like to do.

    But how do I make make a cut-out in the top pcb in order to create a

    cavity? Can I design these three pcb's as a stacked design and only

    create a cut out in one of the pcb's?

     

    I believe what you're looking for is called a "blind via", which is a

    via that begins on one surface of the board, but does not penetrate

    through to the other side - it stops on an inner layer.

     

    Blind vias can be setup in eagle's DRC dialog box.  Since I have never

    used blind vias, I can not purport to know how to set them up.  The

    DRC->Layers tab provides an example with which you can start.

     

    Enjoy,

        - Chuck

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Chuck Huber <chuck.huber@dukepro.com> wrote:

    On 10/05/2011 03:56 PM, Magnus Adelmor wrote:

    >> Hi Jerome,

    >>

    >> Thanks for your help.

    >>

    >> We have a substrate manufacturer who does plugged vias. We will

    >> perform ball bondning on the pad, therefore we need the via filled.

    >>

    >> Your description on how to make cavities is what we would like to do.

    >> But how do I make make a cut-out in the top pcb in order to create a

    >> cavity? Can I design these three pcb's as a stacked design and only

    >> create a cut out in one of the pcb's?

     

    I believe what you're looking for is called a "blind via", which is a

    via that begins on one surface of the board, but does not penetrate

    through to the other side - it stops on an inner layer.

     

    Blind vias can be setup in eagle's DRC dialog box.  Since I have never

    used blind vias, I can not purport to know how to set them up.  The

    DRC->Layers tab provides an example with which you can start.

     

    I believe he is talking about this technique:

    http://blog.screamingcircuits.com/2010/06/how-to-fill-a-via.html

    Eagle does not support that but the manufacturer should be able to do it

    manually.