EAGLE User Support (English) Via without tStop and bStop
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
  • Replies 1 reply
  • Subscribers 178 subscribers
  • Views 1600 views
  • Users 0 members are here
Related

Via without tStop and bStop

autodeskguest
autodeskguest over 17 years ago

Hello,

is there some way to make via between two layers without generating

circle in tStop and bStop layers?

 

Regards

 

Hejduk

 

  • Sign in to reply
  • Cancel
  • Richard_H
    Richard_H over 17 years ago

    Vojtech Hejduk schrieb:

    Hello,

    is there some way to make via between two layers without generating

    circle in tStop and bStop layers?

     

    Regards

     

    Hejduk

     

     

    From http://www.cadsoft.de/faq.htm.en#06062601

     

     

    12. Vias and Solder Stop Mask - How Does it Work?

     

    EAGLE generates by default a solder stop mask for each Via (also for

    Pads and SMDs, of course). This means the Via is free of coating

    material. The solder stop mask is drawn automatically in the layers 29,

    tStop, for the top side and 30, bStop, for the bottom side. The size of

    the solder stop mask can be determined in the Design Rule's Mask

    settings. See the values for Stop. By default the value is fixed to 4

    mils. Minimum and Maximum are set to the same values therefore.

    If you want to have a diameter-dependent mask you could also define a

    certain percentage. The resulting value can be limited by a minimum and

    a maximum.

     

    In order to have vias coated, EAGLE allows you to set the solder stop

    Limit in the Design Rules' Mask tab. Here you can define a value which

    is dependent on the drill diameter of the via. Let's assume you would

    like to set the Limit to 0.012 inch. Now all vias in the layout up to a

    drill diameter of 0.012 inch will be covered with coating material. All

    those vias that have bigger drills will stay uncovered.

    In case you want to have some smaller drilled vias uncovered, you have

    the possibility to select vias out of those that are covered in order to

    uncover them. This can be done with the command CHANGE STOP ON | OFF in

    the Layout Editor. This also works for groups.

     

    By the way: It is allowed to draw areas that should remain free of

    coating material in the tStop/bStop layers directly. But it is not

    possible to delete certain automatically generated solder stop symbols

    there. You have to deal with Limit and CHANGE STOP ON | OFF instead.

     

     

    HTH

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/faq.htm