Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) custom componet pads?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 2 replies
  • Answers 1 answer
  • Subscribers 188 subscribers
  • Views 303 views
  • Users 0 members are here
Related

custom componet pads?

e14 Contributor
e14 Contributor over 14 years ago

Hi, I've tried to search for help on this, but I suppose I'm going about it all wrong so I'm not getting anywhere.

 

I'm trying to make a mini ATO fuse holder package.  here is link to datasheet:  http://www.keyelco.com/pdfs/M55-prod09.pdf  I couldn't find any libraries that already had a mini ATO fuse holder, so I tryied to make my own.  The problem comes when I think I want to have one big pad for both pins on each side and this is the best I can come up with.  It worked fine until I added the supply polygon pour and there's no connecting thermals.  It showes a ratsnest line to the nearest pad on the same net.   I could draw the thermals in hack style, but I'd like my devices that I make to work like thier supposed to.  I also inserted the mounting detail from the datasheet.  All I want is to use the parts with big pads on top and bottom that will connect to the power layer polygon around it.  Thanks, Ben

 

imageimageimage

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Warren,

         Thank you for the reply.  I'll do it that way untill we can edit pads or something equivilant.  Appolagies about the insert instead of attachments, I'll get it next time.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Hi Ben

     

    This is a challenge with Eagle Version 5 (getting fixed somewhat in v6)

    It's not clear if you have a two layer board or multilayer with internal

    power layers. I'll assume a two layer board.

     

    Have a look at my attachment

    Build your package with 4 pads. Your symbol will need to have 4 pins.

    You don't include the polygons for the top and bottom copper in the

    library. You will draw these when you edit the board.

    In the library I added, on a user defined layer, the outlines of the

    polygons that you draw manually on the board. This assists with getting the

    size right and acts as a reminder to do it.

    Next, if  you need to make the solder stop the size of this guiding polygon

    it wont be created automatically so put areas representing the solder stop

    on the tStop and bStop layers. This assumes you want an area larger than

    the pads to solder to. Your thermal problem suggests you are happy with

    just the pad soldered. In which case miss this step.

     

    If this was a SMD part you would need to do the same for the Cream layers

    as well.

     

    Once the part is on the board draw the polygons on the Top and Bottom

    layers, guided by the polygons from the library package.

    Name these polygons the same as the signal on the pads they surround. With

    Thermals set for the polygons the thermals will be created.

     

    A long haul but your there.

    Consider no thermals as they may be rated less than the rating of your

    fuse.

     

    HTH

    Warren

     

     

    ps. When adding files and images when posting at Element14 do not embed

    them in-line. Attach them. as they are not visible on the official CadSoft

    newsgroup forum or EagleCentral site.

    Hopefully a fix for this is going to occur.

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer