Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) How do I change the NET associated with the PAD on the PCB?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 189 subscribers
  • Views 1560 views
  • Users 0 members are here
Related

How do I change the NET associated with the PAD on the PCB?

MontanaEE
MontanaEE over 14 years ago

I have a full schematic and partially routed board.  I need to know how to change the net associated with a pad on the pcb board.  Right now, the board and schematic are not consistent, so no changes I make in the schematics effect the board.

 

All I need to do is change the net name in the board file so that it matches the net in the schematic file.  The schematic nets are correct.  How do I do this?

 

Stephen

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Stephen Doll wrote:

    I have a full schematic and partially routed board. I need to know

    how to change the net associated with a pad on the pcb board. Right

    now, the board and schematic are not consistent, so no changes I make

    in the schematics effect the board.

     

    All I need to do is change the net name in the board file so that it

    matches the net in the schematic file. The schematic nets are

    correct. How do I do this?

     

    Stephen

     

     

    Close the schematic and change the name of the signal on the board.

    Then open the schematic again.

     

    Warren

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • MontanaEE
    0 MontanaEE over 14 years ago in reply to e14 Contributor

    Thanks Warren,

    That put me on the right track, and I think I figured out what happened.  Usually, when I get an inconsistency error, it is because I had either the board or schematic open without the other.  That was not the case this time.

     

    I had both board and schematic open and consistent, started the auto router, and then stopped it at 82%.  I then made changes to the schematic.  When I went to resume the auto route, I got the inconsistency error.  As the signals I changed in the schematics had already been routed on the pcb, that's where the inconsistency was, even though I had the whole project (board and schematic) open at the time I made those changes.

     

    I went into the board and manually connected the pads to the proper net with the Signal command and that brought up the dialog to choose the net names.

     

    So then I ran the auto route again, this time unchecking the box that continued the previous auto routing session.

     

    It's now consistent and autorouting away......

     

    Thanks,

    Stephen

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • MontanaEE
    0 MontanaEE over 14 years ago in reply to e14 Contributor

    Thanks Warren,

    That put me on the right track, and I think I figured out what happened.  Usually, when I get an inconsistency error, it is because I had either the board or schematic open without the other.  That was not the case this time.

     

    I had both board and schematic open and consistent, started the auto router, and then stopped it at 82%.  I then made changes to the schematic.  When I went to resume the auto route, I got the inconsistency error.  As the signals I changed in the schematics had already been routed on the pcb, that's where the inconsistency was, even though I had the whole project (board and schematic) open at the time I made those changes.

     

    I went into the board and manually connected the pads to the proper net with the Signal command and that brought up the dialog to choose the net names.

     

    So then I ran the auto route again, this time unchecking the box that continued the previous auto routing session.

     

    It's now consistent and autorouting away......

     

    Thanks,

    Stephen