Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) How can I create a circular power supply trace?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 188 subscribers
  • Views 513 views
  • Users 0 members are here
Related

How can I create a circular power supply trace?

e14 Contributor
e14 Contributor over 14 years ago

Hi,

I have 40 LEDs arranged radially in a circle, with the anodes all pointing towards the center of the circle. I want to connect the cathodes to Vcc with a fairly heavy power supply trace, but I can't seem to figure out how to do it. I can't rename a circle created on the top layer to "Vcc", and that was y only guess!

 

Any help would be appreciated.

 

Thanks in advance.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Element 14 User wrote on Sun, 11 December 2011 20:35

    I have 40 LEDs arranged radially in a circle, with the anodes all

    pointing towards the center of the circle. I want to connect the cathodes

    to Vcc with a fairly heavy power supply trace, but I can't seem to figure

    out how to do it. I can't rename a circle ...

     

    Actually it sounds like you need a 40 sided polygon, not a circle.  Write a

    little program that writes the Eagle ROUTE command with the 40

    coordinates.

     

    I have a template source module for just this purpose.  It contains

    subroutines for writing out X,Y coordinates in Eagle format, etc.  All I

    would have to do is fill in the 5 lines or so to generate the coordinates.

    If you don't have something like this already set up, take a hour and do

    it.  This same template is useful, for example, for placing a row of pads

    of a IC package.  Another use is to define multiple related library parts,

    like a family of connectors that vary only by the number of pins.  This is

    a really nice thing to have around.  Since speed and efficiency don't

    matter, you can write it in whatever your favorite language is.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    SFOdesigns wrote:

    Hi,

    I have 40 LEDs arranged radially in a circle, with the anodes all

    pointing towards the center of the circle. I want to connect the

    cathodes to Vcc with a fairly heavy power supply trace, but I can't

    seem to figure out how to do it. I can't rename a circle created on

    the top layer to "Vcc", and that was y only guess!

     

    Any help would be appreciated.

     

    Thanks in advance.

     

    There are a few ways butthe most correct way should be as follows.

     

     

    Assuming you have airwires connecting the 40 LED anodes and they are all on

    the circle (9 degrees apart).

    Check HELP for the use of the wire tool and the CTL key to specify an arc

    wire. This applies to ROUTE as well. This creates arcs, you will make 40 of

    them.

     

    Place a MARK in the center of the circular array. This becomes your easy

    reference.

    With ROUTE active, click a LED anode.

    Move the mouse to the MARK, depress the CTL key and left click. A large arc

    will form

    Move the cursor back to the next LED and click on the pad. The short arc

    painted will be of the correct curvature.

     

    HTH

    Warren

     

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    SFOdesigns wrote:

     

    >Hi,

    >I have 40 LEDs arranged radially in a circle,

     

    help net

     

    have a look at the 'curve' and/or '@radius' parameters of the net

    command

    --

     

    Lorenz