Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Feature wish list + need help adjusting renumber ulp
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 188 subscribers
  • Views 558 views
  • Users 0 members are here
Related

Feature wish list + need help adjusting renumber ulp

e14 Contributor
e14 Contributor over 14 years ago

1) What I REALLY need today is a smarter device renumbering ulp or command. Renumbering the whole board works, but the PCB is large and there are many sections. I would like to be able to

a) renumber only the selected group (rather than entire sheet or schematic or board)

b) (better yet) have a smart feature that asks for a distance cutoff, so that all parts within that distance are numbered sequentially, and not only across the X or Y axes.

 

Does anyone know ULP language who could quickly update Eagle's bundled "Renumber" ulp to only use devices that are "In Group" (that is what tech support suggested to me).

 

2) Boy would I LOVE to have a "cell" adjust feature for part groups that are repeated many times on the (a) schematic, and (b) board. By this I mean that I would define a master cell, and then i could easily drop daughter cells that would all change exactly as I change the master cell unless I unlink them from the master. This would be a really, really great feature.

 

Those are my immediate requirements, so any input greatly appreciated. Otherwise, here is the rest of my feature wish list (in time for Christmas image )

 

3) I would love for Eagle to offer the option to beep once autorouting is complete, since I often go to another location and this would be very helpful to know when it is done.

 

4) On busy PCBs with lots of parts, I cannot see the higlighted device when I try to "show" a part, since it is often too small given all the parts, nets, and the size of the PCB being large. It would be GREAT if when parts are shown, would not just highlight slightly brighter, but would actually flash (at least for 5-10 seconds) so I can see them better

 

 

Thanks,

TC

 

Message was edited by: TC Webb

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    I do appreciate all the work that has gone into Eagle, so know that as I offer some more suggestions for my future feature wish list:

     

    1) Although I realize I can set the distance between same signal vias and SMT pads to1mil, I would really love an option that would allow vias to appear inside surface mount pads during autorouting. I often work with tight layout boards, so this feature would be super valuable for space considerations. I understand there might be the slight possiblity of the via drill head making an indent in the PCB surface, but I have never had a problem with this the thousands of times I have moved vias into SMT pads on already working PCBs. As long as it is an option, that would be amazing.

    2) It would be great if for a partially autorouted and then manually stopped PCB if I could somehow run the optimization steps on the routed portion anyway. I say this because I often interrupt the autorouter on complicated boards, and would at least like the option of optimizing routings that have been found.

     

    Happy holidays,

    TC

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Future feature requests continued:

     

    1) Would love to see milticore processor use implemented. I often wait hours for autorouting, in one case, days. Multicore processors are quite common now in CAD industry, so definitely a worthwhile feature and selling poiny.

    2) Would love to have a simple command or button that automatically generates copper pour on any/all layers to the dimensions of the board (minus clearance), with a little dialogue box that asks what signals to use for various pour layers.

     

    Thanks for listening. Interested to hear other users' comments on all the above.

    TC

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Future feature requests continued:

     

    1) Would love to see milticore processor use implemented. I often wait hours for autorouting, in one case, days. Multicore processors are quite common now in CAD industry, so definitely a worthwhile feature and selling poiny.

    2) Would love to have a simple command or button that automatically generates copper pour on any/all layers to the dimensions of the board (minus clearance), with a little dialogue box that asks what signals to use for various pour layers.

     

    Thanks for listening. Interested to hear other users' comments on all the above.

    TC