Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) How on earth do I route a differential pair?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 189 subscribers
  • Views 1034 views
  • Users 0 members are here
Related

How on earth do I route a differential pair?

alexwhittemore
alexwhittemore over 14 years ago

I've searched high and low in docs and the forums, but I still can't figure out how to do it. I have a net named USB_M and a net named USB_P, both of class 0. The best I've figured out how to do is put a meander in one side, and even still that doesn't work because when I try to meander close-together traces, one INVARIABLY tries to overlap the other.

 

So how am I SUPPOSED to route a diff pair?

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to alexwhittemore

    On 12/22/2011 1:31 PM, Alex Whittemore wrote:

    Ok, that's super non-standard, but at least it works. EveryoneI've ever read schematics from in the circuit design business uses P

    (plus) and M (minus). I'd vote that future releases support any obvious

    pairing, P/M, P/N, +/-.

     

    Better question: What do I do about the differing lengths? I can't add meanders since they apply to both traces. This doesn't really fix much. And finally, do I get to set transmission line parameters like impedance (assuming FR-4) or at least spacing?

     

     

    Hi Alex,

     

    I don't know, P(ositive) and N(egative) make sense to me, but not a bad

    suggestion.

     

    You have to use the meanders command but getting it to work require some

    finesse. Right now it doesn't support the ability to specify a specific

    impedance you want to route to, however there are tools available the

    will calculate trace width, length and separation to achieve a specific

    impedance(Saturn PCB's PCB toolkit comes to mind).

     

    Let's say you have two long segments of the differential route and you

    decide that this is where you want to add the meanders to equalize the

    length. Activate the meanders command and left click on the shorter of

    the two traces, where you click is important it's best to click on the

    rightmost(leftmost point) instead of the middle of the trace. So

    assuming you click on the rightmost point move your mouse towards the

    left you should see that if you move far enough away EAGLE will start to

    produce the meanders.

     

    In DRC misc. tab you can setup the Gap Factor and the tolerance on the

    lengths.See HELP MEANDER for more options on the meander command. It

    takes a little bit of play but you'll get it.

     

    hth,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • alexwhittemore
    0 alexwhittemore over 14 years ago in reply to e14 Contributor

    Ok, that's super non-standard, but at least it works. Everyone I've ever read schematics from in the circuit design business uses P (plus) and M (minus). I'd vote that future releases support any obvious pairing, P/M, P/N, +/-.

     

    Better question: What do I do about the differing lengths? I can't add meanders since they apply to both traces. This doesn't really fix much. And finally, do I get to set transmission line parameters like impedance (assuming FR-4) or at least spacing?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    On 12/19/2011 4:18 PM, Alex Whittemore wrote:

    I've searched high and low in docs and the forums, but I still can't figure out how to do it. I have a net named USB_M and a net named USB_P, both of class 0. The best I've figured out how to do is put a meander in one side, and even still that doesn't work because when I try to meander close-together traces, one INVARIABLY tries to overlap the other.

     

    So how am I SUPPOSED to route a diff pair?

     

     

    Hi Alex,

     

    It should be USB_N not USB_M, make sure to use the ROUTE command and not

    the wire command otherwise it won't work.

     

    hth,

     

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    I think you must route one wire at a time...slow & somewhat laborous, but

    possible.  Pehaphas one on  toplayer & the other on a layer below.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.