Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Isolated pins won't connect to a Polygon...
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 189 subscribers
  • Views 625 views
  • Users 0 members are here
  • mx6
  • eagle
  • pin
  • ratsnest
  • pcb
  • led
  • polygon
Related

Isolated pins won't connect to a Polygon...

Steeker
Steeker over 14 years ago

Hi,

 

In the LED library there are symbols for the Cree MX6 LED's that have an isolated pin in the center with thermal vias. 

 

When I place a polygon on layer16, they do not connect to the vias as expected; I need to name the polygon to the same signal name.  However, I cannot find the netname used for this center pin, or the signal name associated with these vias. The LED's only have two pins in the sch symbol, but have 3 pads in the lib footprint.

 

Anyone worked with MX6, or know how to get the isolated vias to connect to the polygon?

 

Thanks!

 

Steve

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    On 12/24/2011 7:39 PM, Steve Krattiger wrote:

    Hi,

     

    In the LED library there are symbols for the Cree MX6 LED's that have an isolated pin in the center with thermal vias.

     

    When I place a polygon on layer16, they do not connect to the vias as expected; I need to name the polygon to the same signal name.  However, I cannot find the netname used for this center pin, or the signal name associated with these vias. The LED's only have two pins in the sch symbol, but have 3 pads in the lib footprint.

     

    Anyone worked with MX6, or know how to get the isolated vias to connect to the polygon?

     

    Thanks!

     

    Steve

     

     

    Hi Steve,

     

         I took a look at this part and have a few suggestions that may help.

    First use the invoke command to make the thermal vias visible in the

    schematic and then connect them together with a net.   Then create your

    polygon and name it the same name as the net used to connect the thermal

    vias in the sch.    Even after doing these steps I was not able to get

    the polygon to connect except by turning thermals off under the polygon

    properties.   Lack of thermals may significantly degrade the ability to

    get good solder contact between the back of the LED and the thermal vias

    and polygon.

     

     

    Jim

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Steeker
    0 Steeker over 14 years ago in reply to e14 Contributor

    Hi Jim,

     

    Thanks for the quick reply on this.  By using the Invoke command on the schematic symbol, that took me to the next step I needed where at least I could name the center conductor and not be guessing.

     

    I connected a net and named it as LED1_TH to keep it isolated.  Once in the PCB, I also named the polygon LED1_TH.  And it still did not connect through.  But on the polygon properties, I went in and turned OFF the checkmark for "Thermals".  That allowed a complete fill of the thermal polygon on Layer16.

     

    Thanks!

     

    Steve

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • Steeker
    0 Steeker over 14 years ago in reply to e14 Contributor

    Hi Jim,

     

    Thanks for the quick reply on this.  By using the Invoke command on the schematic symbol, that took me to the next step I needed where at least I could name the center conductor and not be guessing.

     

    I connected a net and named it as LED1_TH to keep it isolated.  Once in the PCB, I also named the polygon LED1_TH.  And it still did not connect through.  But on the polygon properties, I went in and turned OFF the checkmark for "Thermals".  That allowed a complete fill of the thermal polygon on Layer16.

     

    Thanks!

     

    Steve

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to Steeker

    On 12/26/2011 5:14 PM, Steve Krattiger wrote:

    Hi Jim,

     

    Thanks for the quick reply on this.  By using the Invoke command on the schematic symbol, that took me to the next step I needed where at least I could name the center conductor and not be guessing.

     

    I connected a net and named it as LED1_TH to keep it isolated.  Once in the PCB, I also named the polygon LED1_TH.  And it still did not connect through.  But on the polygon properties, I went in and turned OFF the checkmark for "Thermals".  That allowed a complete fill of the thermal polygon on Layer16.

     

    Thanks!

     

    Steve

     

    Hi Steve,

     

    Glad you got it routed the way you want.   I have worked with some of

    the Luxeon Rebel LEDs which also come with an eagle footprint including

    a nice matrix of thermal vias.   Do not recall having the challenges

    that you experienced so there may be something a little off w/ the MX

    library part although I did not see anything amiss when I quickly looked

    at it w/ the library editor.

     

    Regards,

    Jim