Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) New to Eagle, have some questions.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 190 subscribers
  • Views 576 views
  • Users 0 members are here
Related

New to Eagle, have some questions.

rickford66
rickford66 over 14 years ago

Hi,

I've been using Eagle 6.1 for a couple of days now, going through the tutorial as time allows.  A couple of questions keep coming to mind.

1.  Is there a way to generate a BOM from Eagle?  I don't see how I enter the part numbers and manufacturers information for each part.

2.  In my previous capture/layout software, the schematic and PCB were completely independent of each other.  This allowed me to give the schematic one drawing number, and the PCB another drawing number.  Can I give different drawing numbers to the shematic and PCB in Eagle 6.1?

Thanks.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Am 16.01.2012 23:15, schrieb rickford66:

    1.  Is there a way to generate a BOM from Eagle?

     

    This function is NOT available from the user interface, but CadSoft has

    provided a so-called ULP that can do a rudimentary BOM. You start it by

    typing 'run bom' in EAGLE's command line. I've never used that ULP,

    because it's a bit TOO rudimentary for me, but for a starter, it might

    be OK.

     

    I don't see how I enter the part numbers and manufacturers information for each part.

     

    The above ULP relies on the user creating a small database, which can be

    created from within the program itself. Since documentation of this ULP

    is, errrrm, poor, you might need to fiddle around with it a bit...

     

    2.  In my previous capture/layout software, the schematic and PCB were completely independent of each other.  This allowed me to give the schematic one drawing number, and the PCB another drawing number.

     

    Having schematics and board COMPLETELY independent is NOT such a good

    idea, because it is TOO easy to make errors when changes in one or the

    other are necessary later (one would need to make all changes TWICE and

    pay one HELL of an attention to do everything properly). Therefore,

    schematics and board MUST have the same file name and MUST be loaded at

    the same time.

     

    Can I give different drawing numbers to the shematic and PCB in Eagle 6.1?

     

    Since EAGLE doesn't HAVE the concept of 'drawing numbers' (just file

    names), you would need to put them in as regular text. And of course,

    you can write whatever you want into text fields. But maybe I'm

    misunderstanding something...

     

    Andreas Weidner

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rickford66
    0 rickford66 over 14 years ago in reply to e14 Contributor

    Hmm, I never found it difficult to keep track of the separate files, because the schematic file generated a netlist.  I would load the netlist into the pcb and run a check.  If the pcb didn't match the schematic, I would get errors.  It would tell me what the errors were so I could make corrections.  No big deal there.  Having them linked so tightly is going to take some getting used to.  I wonder how much trouble the BOM things is going to cause me.  Seems weird to me that Eagle would not provide a way to enter part numbers.  I mean, putting a 1206 cap on the board doesn't tell you if the cap is ceramic, pps film, or what.  And, it doesn't tell you who makes it.  Seems like I may have a request to submit for Eagle 6.2.  Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • rickford66
    0 rickford66 over 14 years ago in reply to e14 Contributor

    Hmm, I never found it difficult to keep track of the separate files, because the schematic file generated a netlist.  I would load the netlist into the pcb and run a check.  If the pcb didn't match the schematic, I would get errors.  It would tell me what the errors were so I could make corrections.  No big deal there.  Having them linked so tightly is going to take some getting used to.  I wonder how much trouble the BOM things is going to cause me.  Seems weird to me that Eagle would not provide a way to enter part numbers.  I mean, putting a 1206 cap on the board doesn't tell you if the cap is ceramic, pps film, or what.  And, it doesn't tell you who makes it.  Seems like I may have a request to submit for Eagle 6.2.  Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • rickford66
    0 rickford66 over 14 years ago in reply to e14 Contributor

    Ok, that sounds good.  That is much like my old Tango (DOS) program that allowed the user to create attributes and select those attributes when printing a BOM.  Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to rickford66

    On 17/01/2012 01:34, rickford66 wrote:

    I wonder how much trouble the BOM things is going to cause me. Seems

    weird to me that Eagle would not provide a way to enter part numbers.

    I mean, putting a 1206 cap on the board doesn't tell you if the cap

    is ceramic, pps film, or what.  And, it doesn't tell you who makes

    it.  Seems like I may have a request to submit for Eagle 6.2.

    Thanks.

     

    As well as the name and value, Version 5 introduced user-assignable

    attributes to parts.  This allows you to specify any number of

    additional parameters for each device.  For your example you could, say,

    have a "DETAIL" attribute containing text describing each part ("6.3V

    10% Tantalum", etc).

     

    In particular, attributes are handy for storing supplier order codes and

    many standard devices have an OC_FARNELL attribute already set, giving

    the Farnell order code automatically.

     

    If you use attributes to store additional data that must end up on your

    BoM you will need a BoM generator which pays attention to these. I've

    found the simplest is "bom_with_attributes" but Cadsoft's sites also

    list several others ("attbom", "bom-ex") which I've not tried.

     

    You can get them here:

     

    http://www.cadsoftusa.com/cadsoft-downloads/

     

    Let me know if you find a particularly good one!

     

     

    All the best,

     

     

    Andrew

    0xADF

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Seeker
    0 Seeker over 14 years ago in reply to rickford66

    I use the value and name as separate entities. That is how I keep it clear to me. I can always alter those to fit the BOM later if needed but I try to keep them consistent so it is easier to sort later and add things if I need them. Value is pretty much set (if you use it that way), but name can be whatever you want it to be. That is where I name "type of" for passives, and part number if it is specific.