Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Package vias change sizes when in board layout
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 188 subscribers
  • Views 295 views
  • Users 0 members are here
Related

Package vias change sizes when in board layout

e14 Contributor
e14 Contributor over 14 years ago

I have a connector requiring through holes that are 0.059" (1.5mm) apart from each other, center to center.  The via flange width (outer restring) needs to be 0.0019685" (0.15mm).  I drew this up in created my custom package and device but when I look at it in the board editor all of the vias are touching each other.  I looked in the design rules and could not see how to get this to work.  Is this just too small and not possible?

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    jmoulton wrote:

    I have a connector requiring through holes that are 0.059" (1.5mm)

    apart from each other, center to center. The via flange width (outer

    restring) needs to be 0.0019685" (0.15mm). I drew this up in created

    my custom package and device but when I look at it in the board

    editor all of the vias are touching each other. I looked in the

    design rules and could not see how to get this to work. Is this just

    too small and not possible?

     

    It's possible

     

    When changing the design rules for the restring care must be taken to change

    all three (top,inner,bottom) settings otherwise you will not see the size

    reduction as the largest pad will hide the smaller pads

    (This assumes you have pads set to Green and not the editor background

    colour.)

     

    So assuming, for your connector,  the drill diameter to restring width ratio

    is not abnormal. Change the 'Min' setting to 0.15mm for the pads on all

    layres. If the 0.15mm is greater than 25% (default) of the drill diameter

    the resting will be increased to the minimum (desired) 0.15mm. If it

    calculates to be greater than 0.15mm you would have to reduce the percentage

    figure.

     

    As the DRC settings are global, you should check that this has not impacted

    the other packages in the board editor and resulted in an unresonabley small

    restring

     

    HTH

    Warren

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de