Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) move pins in a library symbol
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 188 subscribers
  • Views 1124 views
  • Users 0 members are here
Related

move pins in a library symbol

e14 Contributor
e14 Contributor over 14 years ago

I'm doing a schematic that has a 16x2 LCD display connecting to an Arduino, when putting in the connecting wires, it crisscross from pin to pin and it looks very messey, how do I move the pins around in the LCD symbols so that I can draw stright wire from Arduino, I tried swap pin but it says the LCD symbol has swaplevel 0 and can not be swaped.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Peter Luke <noreply-82781@element14.com> wrote:

    I'm doing a schematic that has a 16x2 LCD display connecting to an

    Arduino, when putting in the connecting wires, it crisscross from pin to

    pin and it looks very messey, how do I move the pins around in the LCD

    symbols so that I can draw stright wire from Arduino, I tried swap pin

    but it says the LCD symbol has swaplevel 0 and can not be swaped.

     

    Either I am misunderstanding your question or you want to do something very

    wrong. You have to route the crisscross signals if the connecting devices

    have fixed pinout. What you can do with the devices is move, rotate or

    mirror (put on the other side if the pcb).

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Peter Luke <noreply-82781@element14.com> wrote:

    I'm doing a schematic that has a 16x2 LCD display connecting to an

    Arduino, when putting in the connecting wires, it crisscross from pin to

    pin and it looks very messey, how do I move the pins around in the LCD

    symbols so that I can draw stright wire from Arduino, I tried swap pin

    but it says the LCD symbol has swaplevel 0 and can not be swaped.

     

    Either I am misunderstanding your question or you want to do something very

    wrong. You have to route the crisscross signals if the connecting devices

    have fixed pinout. What you can do with the devices is move, rotate or

    mirror (put on the other side if the pcb).

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    I think he is just asking about making the schematic look neater by

    re-arranging the pins on the symbols, not the packages.  I am not sure

    about the Arduino code, however, with the PIC processors (and CCS C

    compiler) I use, there are a number of code examples that let you define at

    the bit level which bit from the processor is which bit on the LCD (allows

    you to drive the LCD with whatever spare pins you have left on the

    processor image  ).  At the board layout level, that would also allow you to

    re-define the pins in the code (sort of like the pin-swap at the gate

    level) to make the board layout work.  Just another thought.

     

    mikey

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.