Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) How do I combine 2 Power Layers on one physical layer (e.g. AVDD/DVDD)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 6 replies
  • Answers 2 answers
  • Subscribers 189 subscribers
  • Views 733 views
  • Users 0 members are here
  • board
  • eagle
  • layers
  • question
Related

How do I combine 2 Power Layers on one physical layer (e.g. AVDD/DVDD)

dcomer
dcomer over 14 years ago

Does any one know of a way, or have a strategy, to combine two power rails on one layer. That is, say for example I want both analog and digital Vdd (say AVdd and DVdd) to exist on a single layer of a 4-layer PCB. The combined layer would have AVdd and DVdd tied together at only one physical point (at a main device GND pin) where the ground and sense lines connect to the layer. For sake of discussion, say layer 1/4 are signal layers, layer 2 is Vss, and layer 3 would be the combined AVdd/DVdd layer. I guess you could think of this as AVdd existing on the top of the layer, and the DVdd drawn on the lower half of the layer with the tie point in the middle.

 

One way to do this would be two separate layer and combine them when I generate the Gerbers. However, I'm not sure how this can be done logically in Eagle allowing Eagle to generate the relieves for the power pins without some type of (yet to be determine layer eqation in the design rule specification.

 

Does this make sense?

 

Thanks,

Dave

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    On 2/1/2012 11:55 AM, Dave Comer wrote:

    Does any one know of a way, or have a strategy, to combine two power rails on one layer. That is, say for example I want both analog and digital Vdd (say AVdd and DVdd) to exist on a single layer of a 4-layer PCB. The combined layer would have AVdd and DVdd tied together at only one physical point (at a main device GND pin) where the ground and sense lines connect to the layer. For sake of discussion, say layer 1/4 are signal layers, layer 2 is Vss, and layer 3 would be the combined AVdd/DVdd layer. I guess you could think of this as AVdd existing on the top of the layer, and the DVdd drawn on the lower half of the layer with the tie point in the middle.

     

    One way to do this would be two separate layer and combine them when I generate the Gerbers. However, I'm not sure how this can be done logically in Eagle allowing Eagle to generate the relieves for the power pins without some type of (yet to be determine layer eqation in the design rule specification.

     

    Does this make sense?

     

    Thanks,

    Dave

     

     

     

    I usually draw 2 polygons on the same layer.  Name one DVdd and one AVdd.

     

    Jim

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    On 2/1/2012 11:55 AM, Dave Comer wrote:

    Does any one know of a way, or have a strategy, to combine two power rails on one layer. That is, say for example I want both analog and digital Vdd (say AVdd and DVdd) to exist on a single layer of a 4-layer PCB. The combined layer would have AVdd and DVdd tied together at only one physical point (at a main device GND pin) where the ground and sense lines connect to the layer. For sake of discussion, say layer 1/4 are signal layers, layer 2 is Vss, and layer 3 would be the combined AVdd/DVdd layer. I guess you could think of this as AVdd existing on the top of the layer, and the DVdd drawn on the lower half of the layer with the tie point in the middle.

     

    One way to do this would be two separate layer and combine them when I generate the Gerbers. However, I'm not sure how this can be done logically in Eagle allowing Eagle to generate the relieves for the power pins without some type of (yet to be determine layer eqation in the design rule specification.

     

    Does this make sense?

     

    Thanks,

    Dave

     

     

     

    I usually draw 2 polygons on the same layer.  Name one DVdd and one AVdd.

     

    Jim

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • dcomer
    0 dcomer over 14 years ago in reply to e14 Contributor

    Jim,

     

    Hum, I didn't think of that (less experience user issue) but I see in the manual pps. 150-153 ("Defining a Copper Plane with a POLYGON" and page 160 ("Supply Layers with Polygons and More than One Signal"). Thanks for the suggestin Jim. That's got me headed in the right direction.

     

    Dave