Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Why Holes have stop layer traces ?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 189 subscribers
  • Views 652 views
  • Users 0 members are here
  • board
  • eagle
  • library
  • pcb
  • gerber
  • layers
  • question
Related

Why Holes have stop layer traces ?

e14 Contributor
e14 Contributor over 14 years ago

Dear all,

 

I wonder why placing a hole in the Layout (manually or by a component which have one (like some connectors)) make a trace in the Stop Layer ?

 

This stop layer is generally used by Gerber file to make the Solder Mask, right ? So why do we need some solder paste inside the PCB hole ?

 

Georges

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Georges Palauqui wrote:

    Dear all,

     

    I wonder why placing a hole in the Layout (manually or by a component

    which have one (like some connectors)) make a trace in the Stop Layer

    ?

     

    This stop layer is generally used by Gerber file to make the Solder

    Mask, right ? So why do we need some solder paste inside the PCB hole

    ?

     

    Georges

     

     

    The stop layers are used to define the Stop Mask. Currently with Eagle it

    automatically applies a solder mask over a regular hole so the solder stop

    material is kept back from the hole edges. As the Solder stop material is

    not very strong this prevents chipping / uplifting of the material around

    the hole circumference. The precision with which the solder mask can be

    placed comes into play a little as well and so this is the industry

    practice.

     

    That said, Eagle should now make that practice an option of each hole. This

    mainly applies to packages but having the option in the board editor would

    not hurt.  With the reducing scale of devices there is an immediate need to

    be able to define a raw hole and not be committed to Eagle /DRC

    defaults/automatic additions. This change must also include preventing  a

    calculated polygon stand back from a hole (distance from shape in dimension

    layer).  Recently the footprint for a MEMS microphone could not be correctly

    created because of this limitation with holes.

     

    The solder paste placement is defined from the Cream layers which are used

    to form the Gerber file for the stencil. Hence, solder paste will not be

    applied to the holes.

     

    I hope this helps

    Warren

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Dear Warren,

     

    this is very detailled answer and I didn't catch everything (because english is not my native language), but I get my important information : Stencil Gerber file should be done using Cream Layer, not Stop Layer....

     

    Thanks a lot,

     

    Georges

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dukepro
    0 dukepro over 14 years ago in reply to e14 Contributor

    On 02/18/2012 01:46 AM, Georges Palauqui wrote:

    Dear Warren,

     

    this is very detailled answer and I didn't catch everything (becasue

    english is not my lative language), but I get my important

    information : Stencil Gerber file should be done using Cream Layer,

    not Stop Layer....

     

    That is correct.  Stencils are produced from the Cream layers.

     

    What may be confusing you is that the stop layers are photographic

    negatives.  That is, stop mask will be everywhere except where traces

    (and circles, and polygons, etc) appear in the on-screen image.  So if

    you see a circle around a hole, that indicates where the solder mask

    will NOT be applied.

     

    Hope this helps.

        - Chuck

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dukepro
    0 dukepro over 14 years ago in reply to e14 Contributor

    On 02/18/2012 01:46 AM, Georges Palauqui wrote:

    Dear Warren,

     

    this is very detailled answer and I didn't catch everything (becasue

    english is not my lative language), but I get my important

    information : Stencil Gerber file should be done using Cream Layer,

    not Stop Layer....

     

    That is correct.  Stencils are produced from the Cream layers.

     

    What may be confusing you is that the stop layers are photographic

    negatives.  That is, stop mask will be everywhere except where traces

    (and circles, and polygons, etc) appear in the on-screen image.  So if

    you see a circle around a hole, that indicates where the solder mask

    will NOT be applied.

     

    Hope this helps.

        - Chuck