Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Off Board Parts
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 9 replies
  • Subscribers 190 subscribers
  • Views 1408 views
  • Users 0 members are here
Related

Off Board Parts

e14 Contributor
e14 Contributor over 14 years ago

Hello my name is Dave and I am new to Eagle and the forum but not PCB design. I make pcbs for guitar effects pedals. These have several off-board connections. I have checked the manual and tutorial to no avail. Without the ability to make off board connections I will have to find software that can handle them. Any ideas or suggestions would be great..

  • Sign in to reply
  • Cancel
Parents
  • robotonics
    0 robotonics over 14 years ago

    Hi Dave

     

    I assume that by 'offboard connections' you are referring to inputs such as pots/pedals etc?

     

    If you could upload a pic of the particular part/s you are having problems with then I may be able to help.

     

    I use Molex connectors myself to make offbaord connections to speakers,power,sensors etc. I find that they are cheap, I can solder them easily, and they are quite tough.

     

    If I am on the right lines let me know and I will help with more detail.

     

    Regards

    David

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to robotonics

    "Without the ability to make off board connections I will have to find software that can handle them."


    "I use Molex connectors myself to make offbaord connections to speakers,power,sensors etc. I find that they are cheap, I can solder them easily, and they are quite tough."

     

    Ding ding ding!!! We have a winner!! What a brilllliant idea!(Yeah, I feel like a dolt now)
    Yeah, just need to do pots, switches etc..

    I've been doing this stuff by hand hand for so long when I finally got behind a computer I kind of lost my mind..

     

    Thank You Very MUCH

    Dave

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Op Tue, 27 Mar 2012 19:33:23 +0200 schreef Dave Cader 

    <noreply-99913@element14.com>:

     

    "Without the ability to make off board connections I will have to find 

    software that can handle them."

     

    >

    "I use Molex connectors myself to make offbaord connections to 

    speakers,power,sensors etc. I find that they are cheap, I can solder 

    them easily, and they are quite tough."

     

    Ding ding ding!!! We have a winner!! What a brilllliant idea!(Yeah, I 

    feel like a dolt now)

    Yeah, just need to do pots, switches etc..

    I've been doing this stuff by hand hand for so long when I finally got 

    behind a computer I kind of lost my mind..

     

    Thank You Very MUCH

    Dave

     

     

    Hello Dave,

     

    Even with the above solution you'll probably want to put the "off-board" 

    parts in the schematic for documentation / clarification purposes.

     

    Andreas Weidner wrote a great ULP for that. With it you can take any 

    component from any Eagle library and 'explode' it, meaning that the 

    schematic symbol will be transformed into just lines on a documentation 

    layer and the PCB package will be removed. So you can add the parts that 

    are not on the board which makes reading the schematic a lot easier.

     

    You can find the ULP from the 'downloads' section on the Cadsoft website.

     

     

    Richard

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gwideman
    0 gwideman over 11 years ago in reply to autodeskguest

    Hi Jorge, and thanks once again for your on-point and crucially useful reply.

     

    I don't know whether to say "Yay" or "ARRRRGGGG!". I guess this feature sneaked in for version 6.2. And though it is documented in both the manual and the in-app Help, it's a bit hard to find unless you know that it's called "External".

     

    Quick note for others: the actual attribute name is the word EXTERNAL with underscore before and after. (Can't show that in this forum, because it's the markup for underscoring the enclosed word -- or maybe there's special additional markup to show it.)

     

    Now, the manual blurb on this (section 8.7 "External Devices without Packages") says: "This attribute [EXTERNAL] has to be created in the library; creating the attribute in the schematic won't work!" The new library device must have only symbol(s), and no package(s).

     

    So actually, the salient thing is to create a library Device that has no Packages; the role of the EXTERNAL "flag" is simply to permit that Device to be used on a schematic, where normally device-without-package is an error.

     

    I guess implementing that was easier than the more user-friendly idea of changing Eagle PCB to ignore schematic Devices with EXTERNAL set on the schematic -- which would have avoided the run-around of having to proliferate new library Devices (in same library? In a new library?) just to get the off-board effect.

     

    Regardless, this is a better-workaround than previous workarounds. Thanks for bringing it to our attention.

     

    -- Graham

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to gwideman

    Instead, I'm finding it easier to maintain an "off-board" library, and

    then:

    • copy a needed component into the off-board library

    • in the library editor, edit the device's symbol(s)* delete the pins

    • replace the pins with wire stubs. Possibly on a different layer, so

    the component is visually distinct from the normal on-board component

     

    • edit the device to delete its package(s)

     

    The resulting library component can be dropped as usual on to a

    schematic, and can be moved around as usual. Its only shortcoming is

    that wires run to its (non) "pins" obviously don't stick. But this is to

    be expected, short of Eagle actually implementing a flag for "real"

    components to be ignored on the PCB, I think.

     

    Any other ideas welcome!

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/157085

     

    Hi Graham,

     

    You can leave the pins in, if you make a device that only has the

    symbol. To define that as an external component simply create an

    attribute name EXTERNAL and EAGLE will treat it as an off board component.

     

    hth,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 11 years ago in reply to gwideman

    Instead, I'm finding it easier to maintain an "off-board" library, and

    then:

    • copy a needed component into the off-board library

    • in the library editor, edit the device's symbol(s)* delete the pins

    • replace the pins with wire stubs. Possibly on a different layer, so

    the component is visually distinct from the normal on-board component

     

    • edit the device to delete its package(s)

     

    The resulting library component can be dropped as usual on to a

    schematic, and can be moved around as usual. Its only shortcoming is

    that wires run to its (non) "pins" obviously don't stick. But this is to

    be expected, short of Eagle actually implementing a flag for "real"

    components to be ignored on the PCB, I think.

     

    Any other ideas welcome!

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/157085

     

    Hi Graham,

     

    You can leave the pins in, if you make a device that only has the

    symbol. To define that as an external component simply create an

    attribute name EXTERNAL and EAGLE will treat it as an off board component.

     

    hth,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • gwideman
    0 gwideman over 11 years ago in reply to autodeskguest

    Hi Jorge, and thanks once again for your on-point and crucially useful reply.

     

    I don't know whether to say "Yay" or "ARRRRGGGG!". I guess this feature sneaked in for version 6.2. And though it is documented in both the manual and the in-app Help, it's a bit hard to find unless you know that it's called "External".

     

    Quick note for others: the actual attribute name is the word EXTERNAL with underscore before and after. (Can't show that in this forum, because it's the markup for underscoring the enclosed word -- or maybe there's special additional markup to show it.)

     

    Now, the manual blurb on this (section 8.7 "External Devices without Packages") says: "This attribute [EXTERNAL] has to be created in the library; creating the attribute in the schematic won't work!" The new library device must have only symbol(s), and no package(s).

     

    So actually, the salient thing is to create a library Device that has no Packages; the role of the EXTERNAL "flag" is simply to permit that Device to be used on a schematic, where normally device-without-package is an error.

     

    I guess implementing that was easier than the more user-friendly idea of changing Eagle PCB to ignore schematic Devices with EXTERNAL set on the schematic -- which would have avoided the run-around of having to proliferate new library Devices (in same library? In a new library?) just to get the off-board effect.

     

    Regardless, this is a better-workaround than previous workarounds. Thanks for bringing it to our attention.

     

    -- Graham