Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) OT: Does anyone have a good, simple random noise generator?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 188 subscribers
  • Views 910 views
  • Users 0 members are here
Related

OT: Does anyone have a good, simple random noise generator?

autodeskguest
autodeskguest over 18 years ago

Does anyone have a schematic for a good, simple random white noise generator.  I

want to use this for audio with a bandwidth up to 25KHz.  I am not particularly

interested in perfect statistical randomness.

 

Thanks in advance.

 

Steve

 

  • Sign in to reply
  • Cancel
  • D_Hersey
    D_Hersey over 10 years ago

    Random number generator 'improved' - BBC News

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • D_Hersey
    D_Hersey over 10 years ago

    Thyratron and a magnet:

     

    http://tubedata.milbert.com/sheets/137/6/6D4.pdf

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 18 years ago

    Tony Rolando wrote:

    "Steve Jacobson" <stevelists@jjworld.com> wrote in message

    news:c16i94trmro9sh8rl01es6maubk9v9fump@4ax.com...

    On Tue, 05 Aug 2008 23:07:28 -0400, Steve Jacobson <stevelists@jjworld.com>

    wrote:

     

    On Tue, 05 Aug 2008 17:44:33 -0700, Gary Gofstein

    <ggofstein@lbl_nospam.gov>

    wrote:

     

    just reverse bias the base emmitter junction of any normal transistor,

    NPN breaks down at about 7V. don't connect the collector. the transistor

    will be useless for any other purpose after this, it will appear to work

    but detailed measurements will show it is out of spec, so throw it away

    if you decide not to use it. 1ma is plenty of current. ac couple the

    transistor voltage to an op amp and voila! true analog white noise.

     

    Gary,

     

    What you are saying is to connect the base-emitter junction of an NPN

    transistor

    to a source greater than 7V.  Connect the base to +7V and the emitter

    to -7V.

    Ground the base and take the white noise off the emitter (coupled with a

    cap).

    Is this correct?  What noise voltage should I expect?

     

    Thanks for your help.  I hope I don't appear too dense.

     

    I will be running the thing at 9V.  Should I be using a current limiting

    resistor?  Also, what would be a good NPN transistor?

     

    Steve

     

    A BC550 is a good place to start. Grab a handful, and select for highest

    noise. I have used 2N3904 as well.

     

     

    However, as Gary wrote make sure it doesn't end up back in the parts

    bin. Snipping off the collector lead or tab would be one way, or paint

    on some gross color (I've used some of my wife's nail polish for that

    but don't tell her ...). If it does end up back in the bin that would be

    a perfect recipe for drustrations months down the road.

     

    --

    Regards, Joerg

     

    http://www.analogconsultants.com/

     

    "gmail" domain blocked because of excessive spam.

    Use another domain or send PM.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 18 years ago

    there is no real danger in reverse biasing the base emitter junction of

    a standard general purpose transistor for this purpose. at 1ma and 7v

    the dissipation will be 7mw, practically nothing. you can experiment

    with the amount of current that produces the best noise.

     

    however, as i mentioned, the transistor should not be used for anything

    else afterward as it will be damaged in regard to speed and noise

    specifications. a zener diode is designed to be reverse biased and will

    take orders of magnitude more power - unfortunately, it will not produce

    as much or as good quality of noise. the noise voltage will vary from

    transistor type to type and within each type from one sample to another,

    but i doubt it will be significant unless you need a calibrated accurate

    level. the zener noise will also vary from unit to unit.

     

    and yes, you must use a resistor to limit the current. if you run it

    from 9v and the junction drops 7v, your resistor should be 2v/1ma or

    2kohm. the voltage will be developed between the emitter and base (which

      you will most likely consider ground) so yes, take the output from the

    resistor emitter connection.

     

    try a gain of 100 as a first guess, though you may need more like 1000.

    it depends upon what final amplitude and frequency range you need. the

    whole problem with these simple noise generators is getting enough

    output, that's why the transistor is better. the more gain you try to

    get from the op amp, the less bandwith you will get. for 25khz, to get a

    gain of 1000 you'd need an op amp with 25Mhz unity gain bandwidth.

    that's not likely a part you have in your junk box. a better bet is to

    use two stages of lower opamp gain if you need it.

     

    it sounds like you are just learning about analog electronics - this is

    a great circuit to teach yourself the fundamentals of analog

    electronics. simple but full of options, like all analog circuits. do

    you think you should use the inverting or noninverting op amp circuits?

    where should you put the gain, is it better to have more noise to start

    with or more amplification? how about power supply rejection, should you

    make a differential connection to the noise source? have fun, try a

    zener diode, try an LED, try different junctions and see for yourself

    what effects they have!

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 18 years ago

     

    "Steve Jacobson" <stevelists@jjworld.com> wrote in message

    news:c16i94trmro9sh8rl01es6maubk9v9fump@4ax.com...

    On Tue, 05 Aug 2008 23:07:28 -0400, Steve Jacobson <stevelists@jjworld.com>

    wrote:

     

    On Tue, 05 Aug 2008 17:44:33 -0700, Gary Gofstein

    <ggofstein@lbl_nospam.gov>

    wrote:

     

    just reverse bias the base emmitter junction of any normal transistor,

    NPN breaks down at about 7V. don't connect the collector. the transistor

    will be useless for any other purpose after this, it will appear to work

    but detailed measurements will show it is out of spec, so throw it away

    if you decide not to use it. 1ma is plenty of current. ac couple the

    transistor voltage to an op amp and voila! true analog white noise.

     

    Gary,

     

    What you are saying is to connect the base-emitter junction of an NPN

    transistor

    to a source greater than 7V.  Connect the base to +7V and the emitter

    to -7V.

    Ground the base and take the white noise off the emitter (coupled with a

    cap).

    Is this correct?  What noise voltage should I expect?

     

    Thanks for your help.  I hope I don't appear too dense.

     

    I will be running the thing at 9V.  Should I be using a current limiting

    resistor?  Also, what would be a good NPN transistor?

     

    Steve

     

    A BC550 is a good place to start. Grab a handful, and select for highest

    noise. I have used 2N3904 as well.

     

    Tony

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 18 years ago

    On Tue, 05 Aug 2008 23:20:16 -0400, Steve Jacobson

    <stevelists@jjworld.com> wrote:

     

    I will be running the thing at 9V.  Should I be using a current limiting

    resistor?  Also, what would be a good NPN transistor?

     

    I would not use a transistor at all.  Reverse biasing a base-emitter

    junction may simply destroy the junction.  You never really know.  It

    may work OK for a hand-built hobby project, but I would not use it in

    anything that I was going to sell.

     

    Instead, use a reversed-biased Zener diode.  They are designed to be

    reverse-biased.  Here is an app note from Maxim (although you can

    probably ignore the use of special low-noise Maxim op amps):

     

      http://www.maxim-ic.com/appnotes.cfm/an_pk/3469

     

     

    Robert Scott

    Real-Time Specialties

    Ypsilanti, Michigan

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 18 years ago

    On Tue, 05 Aug 2008 23:07:28 -0400, Steve Jacobson <stevelists@jjworld.com>

    wrote:

     

    On Tue, 05 Aug 2008 17:44:33 -0700, Gary Gofstein <ggofstein@lbl_nospam.gov>

    wrote:

     

    just reverse bias the base emmitter junction of any normal transistor,

    NPN breaks down at about 7V. don't connect the collector. the transistor

    will be useless for any other purpose after this, it will appear to work

    but detailed measurements will show it is out of spec, so throw it away

    if you decide not to use it. 1ma is plenty of current. ac couple the

    transistor voltage to an op amp and voila! true analog white noise.

     

    Gary,

     

    What you are saying is to connect the base-emitter junction of an NPN transistor

    to a source greater than 7V.  Connect the base to +7V and the emitter to -7V.

    Ground the base and take the white noise off the emitter (coupled with a cap).

    Is this correct?  What noise voltage should I expect?

     

    Thanks for your help.  I hope I don't appear too dense.

     

    I will be running the thing at 9V.  Should I be using a current limiting

    resistor?  Also, what would be a good NPN transistor?

     

    Steve

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 18 years ago in reply to autodeskguest

    On Tue, 05 Aug 2008 17:44:33 -0700, Gary Gofstein <ggofstein@lbl_nospam.gov>

    wrote:

     

    just reverse bias the base emmitter junction of any normal transistor,

    NPN breaks down at about 7V. don't connect the collector. the transistor

    will be useless for any other purpose after this, it will appear to work

    but detailed measurements will show it is out of spec, so throw it away

    if you decide not to use it. 1ma is plenty of current. ac couple the

    transistor voltage to an op amp and voila! true analog white noise.

     

     

    Gary,

     

    What you are saying is to connect the base-emitter junction of an NPN transistor

    to a source greater than 7V.  Connect the base to +7V and the emitter to -7V.

    Ground the base and take the white noise off the emitter (coupled with a cap).

    Is this correct?  What noise voltage should I expect?

     

    Thanks for your help.  I hope I don't appear too dense.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 18 years ago

    just reverse bias the base emmitter junction of any normal transistor,

    NPN breaks down at about 7V. don't connect the collector. the transistor

    will be useless for any other purpose after this, it will appear to work

    but detailed measurements will show it is out of spec, so throw it away

    if you decide not to use it. 1ma is plenty of current. ac couple the

    transistor voltage to an op amp and voila! true analog white noise.