Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Creating new parts - copy and paste?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 188 subscribers
  • Views 723 views
  • Users 0 members are here
  • library
  • create_a_part
Related

Creating new parts - copy and paste?

e14 Contributor
e14 Contributor over 14 years ago

Is there some way to simply open an existing device with the same footprint as your new device and copy the whole enchilada and paste it into your new device and then just edit the pin names and be done with it?  If there is a way, can someone tell me what it is?  And if there isn't, why not?   It seems like this would be the ideal and simplest solution for 99% of every new device one wanted to add to their library.  Or am I missing something?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Op Sun, 01 Apr 2012 01:06:43 +0200 schreef Don French 

    <noreply-101094@element14.com>:

     

    Or am I missing something?

     

     

    It depends...

     

    You don't say what version you are using, with 4.0 copy & paste it is, but 

    I'll assume it's 5.x or higher. In that case:

     

    1) open the library you want to add the device to

    2) find the device you want to copy in the 'control panel'

    3) right click on the device and select 'copy to library'

     

    that's it! start modifying your enchilada ...

     

     

    Richard

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Well that kind of worked. 

     

    I am using 5.5 and am using it for the first time in a very long time - and I never did much library management or part creation when I did use it.  The problem now is that it copied the part to my library but it did not offer  the chance to change the name so now the part I want to use has a completely inappropriate name.  Also, the part I wanted to copy is one of several at the second of the part hierarchy and it only allowed me to copy the top level so I got about 20 parts that I don't want.  I am sure that there must be a way to correct this but I do not find a way to move my new part up to the first level in the hierarchy of my library or to rename it with an appropriate name.  

     

    Wouldn't it be better if there were a menu option to create a new part from an existing part and prompt you to name your new part at that time?    I am feeling frustrated.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Don French wrote:

    Well that kind of worked.

     

    I am using 5.5 and am using it for the first time in a very long time

    - and I never did much library management or part creation when I did

    use it. The problem now is that it copied the part to my library but

    it did not offer the chance to change the name so now the part I want

    to use has a completely inappropriate name.

     

    You can change the name of the device easily.

    In the Device editor view select LIBRARY>RENAME

     

    ...........Also, the part I wanted

    to copy is one of several at the second of the part hierarchy and it

    only allowed me to copy the top level so I got about 20 parts that I

    don't want. I am sure that there must be a way to correct this but I

    do not find a way to move my new part up to the first level in the

    hierarchy of my library or to rename it with an appropriate name.

     

     

    There are no hierarchical levels as in Windows Explorer. What was copied was

    a DEVICE that has many PACKAGE VARIANTS and they in turn can have many

    TECHNOLOGIES

    I feel you identified a package variant and wished for it to be the item you

    select from your library when you do an ADD

    In that case simply delete all unwanted variants and you are left with what

    you need.

    Rename it as required using LIBRARY > RENAME (which actually renames the

    Device if you are in Device editor mode.)

     

    Wouldn't it be better if there were a menu option to create a new

    part from an existing part and prompt you to name your new part at

    that time? I am feeling frustrated.

     

    There have been many requests for changes to the way a user can manipulate

    the libraries. Time will tell if changes are forthcoming.

     

     

    Warren

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Don French wrote:

    Well that kind of worked.

     

    I am using 5.5 and am using it for the first time in a very long time

    - and I never did much library management or part creation when I did

    use it. The problem now is that it copied the part to my library but

    it did not offer the chance to change the name so now the part I want

    to use has a completely inappropriate name.

     

    You can change the name of the device easily.

    In the Device editor view select LIBRARY>RENAME

     

    ...........Also, the part I wanted

    to copy is one of several at the second of the part hierarchy and it

    only allowed me to copy the top level so I got about 20 parts that I

    don't want. I am sure that there must be a way to correct this but I

    do not find a way to move my new part up to the first level in the

    hierarchy of my library or to rename it with an appropriate name.

     

     

    There are no hierarchical levels as in Windows Explorer. What was copied was

    a DEVICE that has many PACKAGE VARIANTS and they in turn can have many

    TECHNOLOGIES

    I feel you identified a package variant and wished for it to be the item you

    select from your library when you do an ADD

    In that case simply delete all unwanted variants and you are left with what

    you need.

    Rename it as required using LIBRARY > RENAME (which actually renames the

    Device if you are in Device editor mode.)

     

    Wouldn't it be better if there were a menu option to create a new

    part from an existing part and prompt you to name your new part at

    that time? I am feeling frustrated.

     

    There have been many requests for changes to the way a user can manipulate

    the libraries. Time will tell if changes are forthcoming.

     

     

    Warren

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de