Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) PCB pool add in reports "air wires still existing"
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 189 subscribers
  • Views 424 views
  • Users 0 members are here
  • eagle
  • layers
Related

PCB pool add in reports "air wires still existing"

Wolfskammer04
Wolfskammer04 over 14 years ago

I installed the above mentioned add in. Actually my board is ready. Then I got this message from that add In. As yo can see in the attached screen shots there are still a couple of very short air wires visible. How can I make them disappear? How serious do I have to take this? I attached some small images to show it.

 

Roland

Attachments:
image
image
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    On Mon, 02 Apr 2012 17:51:41 +0000, Wolfskammer04 wrote:

     

    I installed the above mentioned add in. Actually my board is ready. Then

    I got this message from that add In. As yo can see in the attached

    screen shots there are still a couple of very short air wires visible.

    How can I make them disappear? How serious do I have to take this? I

    attached some small images to show it.

     

    Roland

    I installed the above mentioned add in. Actually my board is ready. Then

    I got this message from that add In. As yo can see in the attached

    screen shots there are still a couple of very short air wires visible.

    How can I make them disappear? How serious do I have to take this? I

    attached some small images to show it.

     

    You're almost certainly OK to send the board to fab.

     

    If you want to get rid of the air wires, you should be able to pick them

    up in manual route mode, then as soon as you drop them they'll be turned

    into traces.

     

    (I'm not stating this well -- I hope I'm making sense).

     

    --

    Tim Wescott

    Control system and signal processing consulting

    www.wescottdesign.com

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Wolfskammer04
    0 Wolfskammer04 over 14 years ago in reply to e14 Contributor

    The problem is, I routed all by hand. They don't exactly snap together as it should be. By what ever reason after even manual routing they stay some mils appart from each other.

    Especially I need a method to get rid of them by some kind of procedure, so that I do not have to pick up every trace.

     

    Thanks Roland

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Wolfskammer04
    0 Wolfskammer04 over 14 years ago in reply to e14 Contributor

    The problem is, I routed all by hand. They don't exactly snap together as it should be. By what ever reason after even manual routing they stay some mils appart from each other.

    Especially I need a method to get rid of them by some kind of procedure, so that I do not have to pick up every trace.

     

    Thanks Roland

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to Wolfskammer04

    On 4/4/2012 1:06 PM, Wolfskammer04 wrote:

    The problem is, I routed all by hand. They don't exactly snap together as it should be. By what ever reason after even manual routing they stay some mils appart from each other.

    Especially I need a method to get rid of them by some kind of procedure, so that I do not have to pick up every trace.

     

    Thanks Roland

     

     

    If you have the autorouter module it should finish off the traces for

    you nicely, just set the routing grid to something like 5 mils and let

    it go to town.

     

    Hth,

    Jorge Garcia