Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Connecting Vcc on schematic
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 177 subscribers
  • Views 1621 views
  • Users 0 members are here
Related

Connecting Vcc on schematic

Former Member
Former Member over 13 years ago

Hello all,

 

Well i am currently using a Breadboard Power Supply 5v/3.3v from Spark fun http://www.sparkfun.com/products/114 and i will be connecting the Vcc pin of the PSU to my schematic (see below). My question is if i insert a pin to the schematic and connect it to Vcc then all i have to do is just attach the bread board Vcc and finished schematic Vcc with hookup wire to obtain my desired voltage of +5v?

 

image

  • Sign in to reply
  • Cancel
  • robotonics
    0 robotonics over 13 years ago

    Hi

     

    Your schematic shows +5V and GND power nets. However, there is no power connector component (DC Jack/Socket) on your schematic. If you are building this all on breadboard then plug the power supply into the breadboard and connect +5V and GND nets accordingly.

     

    Otherwise you will need to add a part to connect to...

     

    So in essence YES, the VCC on breadboard power supply is connected to VCC on your schematic.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 13 years ago in reply to robotonics

    Hello,

    so does that mean that the schematic will have pins created for +5v and GND? or do i need to make them myself to connect the external PSU to the schematic? First time working with Eagle image Thanks for the help image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • robotonics
    0 robotonics over 13 years ago in reply to Former Member

    Hi

     

    Your schematic does not have 'pins' for +5V or GND. All you have at the moment are SYMBOLS for +5V and GND, with NETS connecting to other parts of schematic where +5V and GND are needed.

     

    You need to add a part. Or even two pads to connect wires to.

     

     

     

    So the simplest way for you is to ADD two pads from the wirepad library. image

     

    Then ADD the +5V and GND symbol and wire them together as in the pic.

     

    Then you will have two Through hole pads to solder your +5V and GND wires to, which

     

    can be plugged into the breadboard.

     

     

     

     

     

    Or you could use Header pins...or a DC Jack...or a Molex connector...

     

    So, remember the difference between SYMBOLS and PARTS. Currently you have +5V and GND.... SYMBOLS...PAD1 and PAD2 are actual pads each connected to a schematic SYMBOL.

     

    Does that make sense?...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • Former Member
    0 Former Member over 13 years ago in reply to robotonics

    Thank you so much! that makes perfect sense. great explanation image