Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Board window questions.
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 188 subscribers
  • Views 322 views
  • Users 0 members are here
Related

Board window questions.

e14 Contributor
e14 Contributor over 14 years ago

A couple of maybe "stupid" questions.

 

1)  In the board window.  Sometimes I get a brownish-green "X" usually over a via.   What does this mean?

 

2)  In board window after doing a DRC check.    I get a lot of "overlap" errors.   Can I safely assume these are OK if they are intentional (e.g. ground nets running into/over ground plane and heat sink copper areas)?

 

What is the best way to provide large GND areas for heat sinks?    Draw "rec" on the bottom layer?   How do ground planes get connected to the GND net?   Automatically if they touch/overlap and GND net trace?  They have to be defined explicity?

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    On 21.04.2012 07:50, Joern Paschedag wrote:

    Am 20.04.2012 20:15, schrieb charlesH:

    >> A couple of maybe "stupid" questions.

    >>

    >> 1) In the board window. Sometimes I get a brownish-green "X" usually

    >> over a via. What does this mean?

    >>

    >> 2) In board window after doing a DRC check. I get a lot of "overlap"

    >> errors. Can I safely assume these are OK if they are intentional (e.g.

    >> ground nets running into/over ground plane and heat sink copper areas)?

    >>

    >> What is the best way to provide large GND areas for heat sinks? Draw

    >> "rec" on the bottom layer? How do ground planes get connected to the

    >> GND net? Automatically if they touch/overlap and GND net trace? They

    >> have to be defined explicity?

    >>

    1) Via can be scratched, do a ratsnest.

    2) Only if they are intentional, but you should then mark those as

    accepted.

    3) Use polygons and name them "gnd" if you want to connect them to that

    gnd net. Same names in eagle means a connection even if a net continues

    on a different page.

     

     

    Hi Joern, Hi charlesH

     

    may I add some more information to your answers?

     

    >> 1) In the board window. Sometimes I get a brownish-green "X" usually

    >> over a via. What does this mean?

     

    Such a cross represents an airwire that goes from one layer into

    another layer and the coordinates of start and end point of the airwire

    are the same. For example an airwire from Top to Bottom layer.

     

    If there is a via placed at this location, obviously the via has

    not the name of the signal of the traces. (This could be the reason for

    your overlap errors in DRC, you mentioned in the 3rd question).

     

     

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Am 20.04.2012 20:15, schrieb charlesH:

    A couple of maybe "stupid" questions.

     

    1)  In the board window.  Sometimes I get a brownish-green "X" usually over a via.   What does this mean?

     

    2)  In board window after doing a DRC check.    I get a lot of "overlap" errors.   Can I safely assume these are OK if they are intentional (e.g. ground nets running into/over ground plane and heat sink copper areas)?

     

    What is the best way to provide large GND areas for heat sinks?    Draw "rec" on the bottom layer?   How do ground planes get connected to the GND net?   Automatically if they touch/overlap and GND net trace?  They have to be defined explicity?

     

    1) Via can be scratched, do a ratsnest.

    2) Only if they are intentional, but you should then mark those as accepted.

    3) Use polygons and name them "gnd" if you want to connect them to that

    gnd net. Same names in eagle means a connection even if a net continues

    on a different page.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag