Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) How to create a PowerPad package with the holes includes
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 188 subscribers
  • Views 763 views
  • Users 0 members are here
Related

How to create a PowerPad package with the holes includes

e14 Contributor
e14 Contributor over 14 years ago

image

 

This is a picture I like, with the 8 pin regulator REG+ package with the holes for thermal dissipation. The other side is a ground plane.

There is no space without copper around the holes, so the dissipation is good.

 

I can not do this and I tried a lot. Can you help me?

 

Thank you

Fernando

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Thank you for the answers.

    I am using Eagle 6.1.

     

    I used vias but I would like to have a package...

     

    One test I did was quite good but I got a DRC message like "Layer abuse". I don't remember what I was doing.

     

    I just tried to understand how Eagle works with a little test:

    In the package I created a circle in layer 44 Drills. I can see it on the board editor. I confirmed the CAM use layers 44 and 45 for generating the .TXT file (device EXCELLON). But the resulting TXT file has no hole (acording GERBV). I need an hole with metalic walls (like vias and pads).

    Can someone explain me how the layers work inside the package and how can I simulate holes, vias an pads drawing figures and choosing layers?

     

    Thank you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Lorenz wrote:

    Fernando Silva wrote:

    >> This is a picture I like, with the 8 pin regulator REG+ package with

    >> the holes for thermal dissipation. The other side is a ground plane.

    >> There is no space without copper around the holes, so the

    >> dissipation is good.

    >>

    >> I can not do this and I tried a lot. Can you help me?

     

    assuming you are still on <= 5.x? In that case it's not possible to do

    that in the library.

    --

     

    Lorenz

     

     

    Fair comment for v5  You cannot achieve that  final look by just creating

    the package in the library.

    The 5 air holes could be created in the board  editor using vias (named GND

    or whatever the ground on the other side of your board is named.)

     

    In the library, in a user defined layer, place some markers to act as guides

    for placing  the vias once your package is positioned on the board. Note the

    holes/vias  will not move with the package, which is a shortcoming of the

    technique but easy enough to manage.

     

     

    HTH

    Warren

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Fernando Silva wrote:

    >This is a picture I like, with the 8 pin regulator REG+ package with the holes

    >for thermal dissipation. The other side is a ground plane.

    >There is no space without copper around the holes, so the dissipation is good.

    >I can not do this and I tried a lot. Can you help me?

     

    assuming you are still on <= 5.x? In that case it's not possible to do

    that in the library.

    --

     

    Lorenz