Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) ULP COMMANDS, Layers and Text...
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Subscribers 188 subscribers
  • Views 1378 views
  • Users 0 members are here
Related

ULP COMMANDS, Layers and Text...

e14 Contributor
e14 Contributor over 14 years ago

Hi all,

 

If identacle text exists on two different layers, say layers 25 and 51 and at the same coordinates, what command would one use to change the property of the text on layer 51 without affecting the text on layer 25?  Remember, this is for a ULP that will generate a script to execute the commands.

 

How might one modify the command "CHANGE FONT Fixed (x y);"  to specifically change the text on layer 51 only?  This question assumes all layers are on.

 

Thanks,

ADMsystems

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

     

     

    Fantastic. Thank you.

     

    "DISPLAY NONE layer #" That targets each coordinate on the designated

    layer.

     

    This is a segment of the script file the ULP writes...

     

    EDIT QFN16-4X4.PAC;

    GRID MIL FINEST;

    DISPLAY NONE 51;

    CHANGE FONT Vector (0.000 -125.000);

    CHANGE SIZE 40.000 (0.000 -125.000);

    CHANGE RATIO 16 (0.000 -125.000);

    DISPLAY NONE 51;

    CHANGE FONT Vector (-125.000 -25.000);

    CHANGE SIZE 40.000 (-125.000 -25.000);

    CHANGE RATIO 16 (-125.000 -25.000);

    DISPLAY NONE 25;...etc

     

    The next thing I want to work on is executing all property changes in

    the designated layer without repeating the "DISPLY NONE layer number"

    command for each coordinate.

     

    You dont have to repeat the  DISPLAY NONE 51;

    if all your changes are on that layer. Its the only layer displayed so all

    action happens there for what you are attempting.

    In fact if all your changes are to text on that layer then you can do then

    all at once and not even know where they are positioned.

     

    DISPLAY NONE 51;

    GROUP ALL;

    CHANGE FONT Vector (>0 0);

    CHANGE SIZE 40.000 (>0 0);

    CHANGE RATIO 16 (>0 0);

    DISPLAY LAST;

    GRID LAST;

     

    Warren

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Guest wrote:

     

    Alan Miller wrote:

    Hi all,

     

    If identacle text exists on two different layers, say layers 25 and

    51 and at the same coordinates, what command would one use to change

    the property of the text on layer 51 without affecting the text on

    layer 25? Remember, this is for a ULP that will generate a script to

    execute the commands.

     

    How might one modify the command "CHANGE FONT Fixed (x y);" to

    specifically change the text on layer 51 only? This question assumes

    all layers are on.

     

    Thanks,

    ADMsystems

     

    Remember a script is the same as typing in the command line. What you must

    do in the editor is what must be emulated in the script. Thinking it through

    from that perspective should provide the answer as to what needs to be done.

     

    To specifically target the origin of the text, you should turn off all other

    layers except the layer of interest and then target the co-ordinates of the

    text.

    Good code would assure that there is only one object at that (xy) point on

    that layer.

     

    DISPLAY none 51;

    CHANGE FONT Fixed (x y);"

    DISPLAY last;

     

    The (x y) is provided in units that the board is currently displayed with.

     

    HTH

    Warren

     

     

     

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    Fantastic.  Thank you.

     

    "DISPLAY NONE layer #"  That targets each coordinate on the designated layer.

     

    This is a segment of the script file the ULP writes...

     

    EDIT QFN16-4X4.PAC;

    GRID MIL FINEST;

    DISPLAY NONE 51;

    CHANGE FONT Vector (0.000 -125.000);

    CHANGE SIZE 40.000 (0.000 -125.000);

    CHANGE RATIO 16 (0.000 -125.000);

    DISPLAY NONE 51;

    CHANGE FONT Vector (-125.000 -25.000);

    CHANGE SIZE 40.000 (-125.000 -25.000);

    CHANGE RATIO 16 (-125.000 -25.000);

    DISPLAY NONE 25;...etc

     

    The next thing I want to work on is executing all property changes in the designated layer without repeating the "DISPLY NONE layer number" command for each coordinate.

     

    Thanks again for your help.

     

    Alan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Alan Miller wrote:

    Hi all,

     

    If identacle text exists on two different layers, say layers 25 and

    51 and at the same coordinates, what command would one use to change

    the property of the text on layer 51 without affecting the text on

    layer 25? Remember, this is for a ULP that will generate a script to

    execute the commands.

     

    How might one modify the command "CHANGE FONT Fixed (x y);" to

    specifically change the text on layer 51 only? This question assumes

    all layers are on.

     

    Thanks,

    ADMsystems

     

    Remember a script is the same as typing in the command line. What you must

    do in the editor is what must be emulated in the script. Thinking it through

    from that perspective should provide the answer as to what needs to be done.

     

    To specifically target the origin of the text, you should turn off all other

    layers except the layer of interest and then target the co-ordinates of the

    text.

    Good code would assure that there is only one object at that (xy) point on

    that layer.

     

    DISPLAY none 51;

    CHANGE FONT Fixed (x y);"

    DISPLAY last;

     

    The (x y) is provided in units that the board is currently displayed with.

     

    HTH

    Warren

     

     

     

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer