Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Eagle 5.1.1 wires/lines not editable
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 188 subscribers
  • Views 762 views
  • Users 0 members are here
Related

Eagle 5.1.1 wires/lines not editable

e14 Contributor
e14 Contributor over 14 years ago

Hi, forum,

 

I inherited a project from someone who left the company a while back. when i tried to do some modifications to the dimention and keepout layer, i have the trouble not being able to edit any of the lines. these are visible boarders/fills/polygons but no way to click through or get high-lighted, just as if they do not exist. Any obvious reason that can cause such lock down?

 

Thanks

GZ

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Guoliang Zhang wrote:

    Hi, forum,

     

    I inherited a project from someone who left the company a while back.

    when i tried to do some modifications to the dimention and keepout

    layer, i have the trouble not being able to edit any of the lines.

    these are visible boarders/fills/polygons but no way to click through

    or get high-lighted, just as if they do not exist. Any obvious reason

    that can cause such lock down?

     

    Thanks

    GZ

     

     

    Maybe the bare board was built as a library part and potentially it is

    "Locked" . If you cannot get an Information dialog to display for the

    dimension wire then this is likely.

     

    HTH

    Warren

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    If that is the case, when I generate a part list from the File/Export... option, do I see the library from which this board is residing? I did just that and could not find the board listed in any place of that list. Is there a way to tell where the board library is or what name it is? The brd file is binary, I have no way to figure out the hierachy.

     

    Thanks

    GZ

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Now actually I can run a ULP called exp-project-lbr.ulp to generate a library which does contains the mechanical only part that represents the board. but still after i modified the library, use the library, update the board layout, the board does not get changed. even worse, if I add this as part from the schematic, a few extra board outlines are added to the layout and I cannot delete them. what kind of 'part' this is? how can I move or delete or edit it properly?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Robert Pearce wrote:

    On Wed, 20 Jun 2012, Warren Brayshaw wrote to us saying :

    >> The board may not get changed after a library modifircation for a

    >> number of reasons

     

    There's another one, I think, at least on V4.16 (it may have changed)

     

    When you run exp-project-lbr it creates a library. When you have

    "USE"d this library and updated all, even with the directory order

    and unique names sorted, this does not cause any existing components

    to be taken from the new library. So, for example, all the resistors

    are still associated with the RCL library.

     

    I don't know if that's a real problem for a component that originally

    came from a library that you don't have.

    --

    Rob Pearce                       http://www.bdt-home.demon.co.uk

     

     

     

    This, I think, is a caused by one of the conditions I mentioned.

     

    exp-project-lbr  can export to multiple or a single library.

     

    Exporting to multiple libraries

    The parts on your board still refer to a library called RCL and will only

    update from a library called RCL

    With this in mind, to have them update, they have to find the new library

    named RCL before finding the old RCL

    This means the path to the new libraries, created with the export, has to be

    in the directory path before the path to the old RCL. If not the old RCL

    will provide the detaile for the update.

     

    Exporting to a single library

    Here you generate a single library with a new name.

    An update all will not look into it as the board components never know of

    this library.

     

    Warren

     

     

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    On Wed, 20 Jun 2012, Warren Brayshaw wrote to us saying :

    >The board may not get changed after a library modifircation for a number of

    >reasons

     

    There's another one, I think, at least on V4.16 (it may have changed)

     

    When you run exp-project-lbr it creates a library. When you have "USE"d

    this library and updated all, even with the directory order and unique

    names sorted, this does not cause any existing components to be taken

    from the new library. So, for example, all the resistors are still

    associated with the RCL library.

     

    I don't know if that's a real problem for a component that originally

    came from a library that you don't have.

    --

    Rob Pearce                       http://www.bdt-home.demon.co.uk

     

    The contents of     | All power corrupts, but we need electricity.

    this message are    |

    purely my opinion.  |

    Don't believe a     |

    word.               |

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    On Wed, 20 Jun 2012, Warren Brayshaw wrote to us saying :

    >The board may not get changed after a library modifircation for a number of

    >reasons

     

    There's another one, I think, at least on V4.16 (it may have changed)

     

    When you run exp-project-lbr it creates a library. When you have "USE"d

    this library and updated all, even with the directory order and unique

    names sorted, this does not cause any existing components to be taken

    from the new library. So, for example, all the resistors are still

    associated with the RCL library.

     

    I don't know if that's a real problem for a component that originally

    came from a library that you don't have.

    --

    Rob Pearce                       http://www.bdt-home.demon.co.uk

     

    The contents of     | All power corrupts, but we need electricity.

    this message are    |

    purely my opinion.  |

    Don't believe a     |

    word.               |

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Robert Pearce wrote:

    On Wed, 20 Jun 2012, Warren Brayshaw wrote to us saying :

    >> The board may not get changed after a library modifircation for a

    >> number of reasons

     

    There's another one, I think, at least on V4.16 (it may have changed)

     

    When you run exp-project-lbr it creates a library. When you have

    "USE"d this library and updated all, even with the directory order

    and unique names sorted, this does not cause any existing components

    to be taken from the new library. So, for example, all the resistors

    are still associated with the RCL library.

     

    I don't know if that's a real problem for a component that originally

    came from a library that you don't have.

    --

    Rob Pearce                       http://www.bdt-home.demon.co.uk

     

     

     

    This, I think, is a caused by one of the conditions I mentioned.

     

    exp-project-lbr  can export to multiple or a single library.

     

    Exporting to multiple libraries

    The parts on your board still refer to a library called RCL and will only

    update from a library called RCL

    With this in mind, to have them update, they have to find the new library

    named RCL before finding the old RCL

    This means the path to the new libraries, created with the export, has to be

    in the directory path before the path to the old RCL. If not the old RCL

    will provide the detaile for the update.

     

    Exporting to a single library

    Here you generate a single library with a new name.

    An update all will not look into it as the board components never know of

    this library.

     

    Warren

     

     

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de