Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) DRC check for via diameter (not drill diameter)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 188 subscribers
  • Views 741 views
  • Users 0 members are here
  • drc
Related

DRC check for via diameter (not drill diameter)

e14 Contributor
e14 Contributor over 14 years ago

Hi,

 

Even though I knew better, I again made a PCB with via's with 0.8 mm drills with the default diameter, resulting in too small a pad (I make the boards myself so I don't have through-hole plating, and pads that are too small can tear off).

 

So, I was going to make a design rule that checks via diameter, but I couldn't find any. Is that right, or am I overlooking something?

 

I use Eagle 6.2

 

Thanks

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Thank you, this is exactly what I needed. Might do it to pads as well, as far as it allows me to still run wires between 0.1 grids.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Wiebe Cazemier wrote:

    Hi,

     

    Even though I knew better, I again made a PCB with via's with 0.8 mm

    drills with the default diameter, resulting in too small a pad (I

    make the boards myself so I don't have through-hole plating, and pads

    that are too small can tear off).

     

    So, I was going to make a design rule that checks via diameter, but I

    couldn't find any. Is that right, or am I overlooking something?

     

    I use Eagle 6.2

     

    Thanks

     

     

    The DRC not only checks dimensions but also causes sizes to happen.

    Your issue would be solved by setting, within the DRC, the 'restring' value

    for vias.

    Doing that correctly will enable a minimum copper area around the via hole

    for small drill sizes.

    Set the DRC/ Restring / Via /  Outer / Min value to the width of copper you

    want.

     

    HTH

    Warren

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer