Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) How to connect V+ and GND pins on a LM324N Op Amp
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 190 subscribers
  • Views 5464 views
  • Users 0 members are here
Related

How to connect V+ and GND pins on a LM324N Op Amp

scott216
scott216 over 14 years ago

I'm just learning to use Eagle software.  I have a schematic that uses a LM324NE3.LM324NE3. Op-Amp.  When I add this part, eagle lets me add 4 op-amp traingles to the schematic, but I can't figure out how to connect wires to V+ (pin 6) and GND (pin 11) because they are not shown on the schamatic diagram.  My circuit actually requires +5 volts and -5 volts for the LM324. I'm using a MAX1044 to create the -5 Volts which will go to LM324 pin 11 (ground pin).  How do I wire the V+ and GND pins on the LM324NE3.LM324NE3.?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    On 7/30/2012 12:03 AM, Scott Goldthwaite wrote:

    I'm just learning to use Eagle software.  I have a schematic that uses a LM324NE3.LM324NE3. Op-Amp.  When I add this part, eagle lets me add 4 op-amp traingles to the schematic, but I can't figure out how to connect wires to V+ (pin 6) and GND (pin 11) because they are not shown on the schamatic diagram.  My circuit actually requires 5 volts and -5 volts for the LM324. I'm using a MAX1044 to create the -5 Volts which will go to LM324 pin 11 (ground pin).  How do I wire the V and GND pins on the LM324NE3.LM324NE3.?

     

     

    Hi Scott,

     

    Use the INVOKE command to bring in the hidden power pins. Several of

    EAGLE's libraries have the power supply pins hidden so you can use the

    invoke command to bring them into the design and connect them explicitly.

     

    Let me know if there's anything else I can do for you.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    On 7/30/2012 12:03 AM, Scott Goldthwaite wrote:

    I'm just learning to use Eagle software.  I have a schematic that uses a LM324NE3.LM324NE3. Op-Amp.  When I add this part, eagle lets me add 4 op-amp traingles to the schematic, but I can't figure out how to connect wires to V+ (pin 6) and GND (pin 11) because they are not shown on the schamatic diagram.  My circuit actually requires 5 volts and -5 volts for the LM324. I'm using a MAX1044 to create the -5 Volts which will go to LM324 pin 11 (ground pin).  How do I wire the V and GND pins on the LM324NE3.LM324NE3.?

     

     

    Hi Scott,

     

    Use the INVOKE command to bring in the hidden power pins. Several of

    EAGLE's libraries have the power supply pins hidden so you can use the

    invoke command to bring them into the design and connect them explicitly.

     

    Let me know if there's anything else I can do for you.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • scott216
    0 scott216 over 14 years ago in reply to e14 Contributor

    Thanks. It's one of those things that's easy once you know how.