Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Power Planes (Polygon Tool Questions)
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 190 subscribers
  • Views 578 views
  • Users 0 members are here
  • polygon
Related

Power Planes (Polygon Tool Questions)

e14 Contributor
e14 Contributor over 13 years ago

Hello, I have a question about using the polygon tool.

 

I just finished a design where I had half of my top layer as a VDD plane, and half of my top layer and a GND plane. On the VDD half of the board, I had a power plug and a voltage regulator with an associated capacitor. What I wanted to do was run a thick trace from the regulator to the capacitor and then have the VDD plane connected from the capacitor. This would make it so that everything connected to that plane would be "downstream" of the capacitor. However, because the trace to the capacitor and the plane had the same net (electrically they are connected) the plane simply overlapped the trace removing the "downstream" aspect. To solve the problem I had to make another polygon with a different net with a weird shape that followed the trace and gave it a higher rank so that the VDD plane couldn't get near the trace. Is there a more elegant way of solving this problem?

 

I also had a similar problem where I wanted part of the plane to have islands and part of it to not have islands. In order to make some of the islands disappear I had to make extra polygons with different nets.

 

Is there a guide to using the polygon tool that covers some of the more advanced features anywhere? Does anyone have experience with this problems?

 

Thank you.

  • Sign in to reply
  • Cancel
Parents
  • Lupo
    0 Lupo over 13 years ago

    Good question. I think actually the best way to do that is to use many smaller VDD areas in order to have the place to connect also the VDD trace. I'm not sure there is a more elegant and faster function or some settings to perform this kind of connections in such way. Let's see if one of the Eaglecad software designers can solve this doubt.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Lupo
    0 Lupo over 13 years ago

    Good question. I think actually the best way to do that is to use many smaller VDD areas in order to have the place to connect also the VDD trace. I'm not sure there is a more elegant and faster function or some settings to perform this kind of connections in such way. Let's see if one of the Eaglecad software designers can solve this doubt.