Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Eaglecad 6.3 causes unhandled exception in windows xp
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 188 subscribers
  • Views 488 views
  • Users 0 members are here
Related

Eaglecad 6.3 causes unhandled exception in windows xp

e14 Contributor
e14 Contributor over 13 years ago

Hello

 

I would like to ask for help with Version 6.3. I have installed this version and am inprocess of upgrading all projects from version 5.10. When adding parts a schematic, clicking the cancel button causes windows to generate the error message "An unhandled win32 exception has occurred in eagle.exe[3524]. Earlier versions of Eaglecad work without issues.

 

I am not sure where to look for the problem. What have I missed in the installation process?

 

Any help is greatly appreciated

 

Thank You!

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Richard,

     

    Any updates as to what to look for to solve this problem? I am still unable to use version 6.3 on xp without the program causing an unhandled exception error.

     

    I have removed all versions of Eaglecad except 6.3 and still get the same errors.

     

    Thank You

     

    George

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Richard,

     

    Thank You for the reply.

     

    I have been testing version 6.3 on different platforms and find that version 6.3 will crash unexpectedly on windows 7 (32 or 64 bit). This may occur at any time and there is no particular command sequence that I can find that will cause the crash. I have seen the problem on saving a file, routing a board, and moving parts in the schematic.

     

    The xp problem seems to be related to inserting from a library, but I have crashed the program by moving parts in the schematic.

     

    A further observation is that 6.3 seems to crash in a similar manner on mulitple machines I have access. to

     

    If it will help I can post the event log from a win 7 64 bit machine

     

    Thank You

     

    George

     

     

    Here is the event log from Win7 64 bit on program crash

    Faulting application name: eagle.exe, version: 0.0.0.0, time stamp: 0x5072b003

    Faulting module name: unknown, version: 0.0.0.0, time stamp: 0x00000000

    Exception code: 0xc0000005

    Fault offset: 0x00000000

    Faulting process id: 0x170c

    Faulting application start time: 0x01cdb0ad4157f0d0

    Faulting application path: C:\Program Files (x86)\EAGLE-6.3.0\bin\eagle.exe

    Faulting module path: unknown

    Report Id: b362eb96-1ca0-11e2-8cc4-0025646a0ff2

     

    Fault bucket , type 0

    Event Name: BEX

    Response: Not available

    Cab Id: 0

     

    Problem signature:

    P1: eagle.exe

    P2: 0.0.0.0

    P3: 5072b003

    P4: StackHash_e98d

    P5: 0.0.0.0

    P6: 00000000

    P7: 00000000

    P8: c0000005

    P9: 00000008

    P10:

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    On 12.10.2012 01:39, shmuncle wrote:

    Hello

     

    I would like to ask for help with Version 6.3. I have installed this

    version along and am inprocess of upgrading all projects from version

    5.10. When adding parts a schematic, clicking the cancel button

    causes windows to generate the error message "An unhandled win32

    exception has occurred in eagle.exe[3524]. Earlier versions of

    Eaglecad work without issues.

     

    I am not sure where to look for the problem. What have I missed in

    the installation process?

     

    Any help is greatly appreciated

     

    Thank You!

     

     

    I tried this here and don't experience this problem......

     

    Could you check the settings in the Options/Directories menu for

    the Library path. Is it pointing to the current EAGLE 6.3 libraries?

    If not, please adjust it, open a schematic and try it again.

     

    Does this happen all the time you press the Esc key?

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/training/faq/