Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Wire Link question - Eagle Newbie
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 188 subscribers
  • Views 1858 views
  • Users 0 members are here
  • board
  • pad
  • pads
  • autorouter
  • pcb
  • wire
  • pour
  • layer
  • link
Related

Wire Link question - Eagle Newbie

e14 Contributor
e14 Contributor over 14 years ago

New to Eagle and loving it. I'm developing a single sided board and have used manual and auto routing to get an 87% finished board. I'd like to add wire links in to jump a few islands

 

For instance, unconnected GND Planes and a few components with placements unable to route directly. I can add pads to the layout and connect to components but how do I signify to Eagle that these are connected (with a wire link) and hence, remove the air wires? And, how do I add pads to the ground plane and a link for the same purpose. When I add a pad to the ground plane, and do a Rats Nest, the pads are isolated.

 

All help gratefully appreciated.

 

TIA Steve

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    Well, I've done more digging and found an answer. If you manually lay 'Wires' and Vias, you can add a 'link', actually a trace, on the top layer. this is seen as a valid link by Eagle so when you do a Ratsnest, it tidys up the air wires. I've searched nigh on 5 days for this info!

     

    Any other suggestions will still be welcome. I've lots to learn!

     

    Steve

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Il 03/11/2012 00:34, Steve Smith ha scritto:

     

    Well, I've done more digging and found an answer. If you manually lay 'Wires' and Vias, you can add a 'link', actually a trace, on the top layer. this is seen as a valid link by Eagle so when you do a Ratsnest, it tidys up the air wires. I've searched nigh on 5 days for this info!

     

    Any other suggestions will still be welcome. I've lots to learn!

     

     

    It's the right way. In fact the wire links are placed on the top layer.

    If you make a double sided board they will be traces, actually. With a

    single side board you make them manually, but EAGLE doesn't know that image

     

    Marco

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to e14 Contributor

    Il 03/11/2012 00:34, Steve Smith ha scritto:

     

    Well, I've done more digging and found an answer. If you manually lay 'Wires' and Vias, you can add a 'link', actually a trace, on the top layer. this is seen as a valid link by Eagle so when you do a Ratsnest, it tidys up the air wires. I've searched nigh on 5 days for this info!

     

    Any other suggestions will still be welcome. I've lots to learn!

     

     

    It's the right way. In fact the wire links are placed on the top layer.

    If you make a double sided board they will be traces, actually. With a

    single side board you make them manually, but EAGLE doesn't know that image

     

    Marco