I need to use a SMD connector which requires two pads per contact (Molex
52610). The problem is how to make Eagle aware of multi-part SMD pads.
I have a 10-contact connector which has 20 pads in two rows (2x10 pads).
Each contact in the connector is shaped so that it uses two separate
pads, on in each end of the contact. I know I could solve the problem by
making a 20-contact connector and then connecting the contacts pairwise
in the schematic editor. Unfortunately, this would lead to a messy
schematic and also ruin interchangeability with 10-pin FPC connectors.
Is there some smd pad naming trick which would help here? I have named
the pads 1,2,...10 and 1b,2b,...10b, but is there some way to name the
pads so that Eagle would recognize them to belong to the same potential?
Or is there some other way to connect several pads to one signal?
I do not think this problem is unique. For example, many dfn packages
have an exposed ground pad in the middle (either for better heat
conduction or for better GND contact), and that pad is seldom drawn in the
schematic.
TIA,
- Ville
--